Part Number: TLV2170 Other Parts Discussed in Thread: TLV9302 Hello team,
Do we have the specification for "Input current noise density"? If we have, please share with me.
Best regards,
Shotaro
Part Number: TLV2170 Hi, Staff
Distance of each Sprocket Holes
TLV2170(IDR) Data Sheet (SBOS782A) There is a figure of "QUADRANT ASSIGNMENTS FOR PIN1 ORIENTATION IN TAPE" on page29.
Question: Please tell me the spacing dimension of Sprocket Holes…
Part Number: TLV2170 The TLV2170 whithstands at output only short-circuit to ground. We need also short-circuit to plus. Could we put some Rout resistor to output similar as at capacitive loud? How big must be the resistor? Would you recomend me some…
Part Number: TLV2170 Other Parts Discussed in Thread: TINA-TI Tool/software: TINA-TI or Spice Models HI Team
I found the TLV2170IDR but could not get the spice model work on Simetrix.
I ended up using Tina-TI, but do you know why the PSpice model I…
Part Number: TLV2170 Hi team,
Would it be possible to obtain min/max values for input common mode capacitance value for TLV2170 amplifier ?
My customer want to calculate the CMRR knowing the source resistor values (100k). There is only a typ value in…
Part Number: XTR111 Other Parts Discussed in Thread: LM358 , TLV2170 , TLV9302 , OPA2170 , LM7705 , TINA-TI hello. I've been trying to get 4-20ma output with xtr111 for a while. I'm applying the output of lm358, which has a gain of 10, giving 0-10v output…
Suzuki-san,
Because power supply is 5V, I suggest LM358LV or TLV9002 as the low cost solutions. To support more supply voltages, I suggest TLV9302 or TLV2170. The OPA2990 should also work well.
Hi Toon,
For a high voltage voltage-follower, you could choose a newer CMOS op-amp like the OPA2170 or TLV2170. The TL062 might also be a good choice.
Hope that helps,
Paul
Kevin,
Your input common mode on pin 3 is 4V which is fine for RC4558. Into a lighter load RC4558 has a better VOH than LM358, especially at low temperature. Typical RC4558 VOH at 25C, is VCC - 0.75V - IOUT * 205 ohms (+2mV/C); this is better than LM358…
Hello,
Here's a link to a good design guide for non-inverting amplifier circuits. The LMC662 is a good amp but there are much newer alternatives which perform better for lower costs.
For +1.8V - 5.5V supplies look at the TLV9002 (1MHz) or TLV9062…