Part Number: TLV2544
Hello Team, We are planning to use the ADC TLV2544 for one of our applications. The ADC will be sampling at a rate of 200ksps. What will be the total latency of the ADC?
What is the throughput of the ADC? Based on a rough calculation…
Other Parts Discussed in Thread: TLV2544Q I am having a problem with the TLV2544Q 12-Bit Serial ADC. The LSB of the conversion result is always 0 when the measured voltage is at the higher end of the measurement range. Consequently, the ADC acts properly…
Part Number: TLV2548-EP Other Parts Discussed in Thread: TLV2548 , TLV2544 , TLV1544
Is the number of channels of TLV2548-EP 4 or 8?
The datasheet says:
"The 4/8 analog inputs and three internal test inputs are selected by the analog multiplexer depending…
Yes. 1st pic is SDI and 2nd pic is SDO.
power up and initialization requirements:
Determine processor type by writing A000h to the TLV2544/48 (CS must be toggled)
----> Yes.
Configure the device (CS must make a high-to-low transition, then can be held…
Part Number: ADS1119 Other Parts Discussed in Thread: ADS7924 , TLV2544 , ADS8201 , ADS7142 , TLC2574 hi sir
I need a solution ,spec as below
ADC+EEPROM,2-channel( EEPROM 1Kbyte ADC 12bit~16bit .
power : 5.5V (TYP)or 5 .5V
Hi Seb,
Take a look at the TLV2544 or TLV2548 for single ended signals. If you need a faster device, we also have the THS1206 which can accommodate either single ended or differential inputs. Many of our parts that include a REFM, have a limited range…
Other Parts Discussed in Thread: ADS7824 , ADS7841 , ADS7924 , TLV2544 , TLC2554 , ADS8508 , ADS8519 , ADS8512 I am looking for a replacement for the ADS7824P.
I need the same input and conversion capability (number of bits) but I need a smaller package (serial…
Other Parts Discussed in Thread: TLV2544 , ADS1015 , ADS1115 Good afternoon - hopefully this isn't too tricky of a question:
We desire a 4-input 12-bit ADC controllable entirely over three-wire serial communication (RxD, TxD, GND):
Input voltage…
Hi Prabhakar,
The EOC/INT would be used by your controller as an interrupt source. You might find the code examples for the TLV2544 associated with the following app note useful:
http://focus.ti.com/analog/docs/litabsmultiplefilelist.tsp?literatureNumber…