Part Number: TLV2548
Could you please advise the status of below parts, they were earlier not found on website but are 'Active' now.
CC1260RGZR TLV2548MPWREP
Thank you in advance for your help!
If your ISO_VDD_5V0 is stable, then the only other thing I can think of is that somehow you are feeding SDO into a resistive divider or high impedance node.
Part Number: TLV2548-EP Other Parts Discussed in Thread: TLV2548 , , TMS320F28377D Hello,
I have a question about the TLV2548 chip, which behaves differently depending on whether it is operating at room temperature or at a low temperature.
We are using…
Part Number: TLV2548 There was a reference to an application note in one of the posts ( SLAA093a ) that had sample code for the setup and acquisition from the TLV254x ADCs. I can't find that AN. Is there another reference that has example / reference…
Part Number: TLV2548 Hi TI Team,
We are using TLV2548CDWR to read analog voltage and current from different channels. We have some queries as part of that which is listed below.
1. In the datasheet it is mentioned like the total conversion time is 3.5us…
Part Number: TLV2548 I have an application where I periodically send configuration information to the ADC (after sampling 4 channels).
The data sequence into the ADC goes as follows. Config Info, Channel 0, Channel 1, Channel 2, Channel 3, (repeat message…
Part Number: TLV2548-EP Other Parts Discussed in Thread: TLV2548 , TLV2544 , TLV1544
Is the number of channels of TLV2548-EP 4 or 8?
The datasheet says:
"The 4/8 analog inputs and three internal test inputs are selected by the analog multiplexer depending…
Part Number: TLV2548-EP Other Parts Discussed in Thread: TLE2022 , TLV2548 I am getting some unintended adjacent channel to channel coupling between an input channel of maximum input voltage (say 4.095V), and the adjacent channel of 0V.
The inputs to the…
Part Number: TLV2548-EP
The Device has only one supply pin. What is the SDO and EOC/nINT voltage level? The that sheet shows the VOH (min). But it does not tell me if the pin has no load. In normal usage, the input port of its master device is in high…
Part Number: TLV2548-EP Other Parts Discussed in Thread: TMS570LC4357 ,
Hello,
I would like to integrate external ADC TLV2548-EP with TMS570LC4357 SPI4 channels.
Please confirm whether the unused FS, nCSTART and nPWDN can be tied to VCC pin.
Attached schematics…