Part Number: TLV2553 Other Parts Discussed in Thread: TLV2556 , ADS7952 Hi team,
I am considering TLV2553 as a replacement for TLV2556. I am setting data to the internal configuration register (CFGR2) of the TLV2556IPW for external reference mode and EOC…
Part Number: TLV2556 Other Parts Discussed in Thread: TLV2553 , , TLC2543 Hello we are looking to use the TLV2556 and TLV2553 as alternates for TLC2543.
With TLV2556 we have had issues with the CFGR2 being set to default mode (reads only channel 0 regardless…
Part Number: TLV2553 Other Parts Discussed in Thread: LM358 Hi,
Need design review of the below design:
All SENSORx_VOLTAGE values are between 0 - 3.3V.
Thanks,
Shyam
Part Number: TLV2553 Summary of Problem:
I am getting inaccurate readings using the TLV2553 in 8-bit precision mode despite verifying all of my connections and transmitting in 8-bit mode using CS as illustrated in Figure 3 of rev C of the datasheet. I…
Hi Brian,
Glad we were able to resolve the issue! Do let us know if we can help with anything else.
For anyone else interested, the issue (in a nutshell) turned out to be a missing feedback resistor around one of the drive amps.
Part Number: TLV2553 Hi I'm a new hand to use ADC tlv2553,Although i watch datasheet, i am unable to write code for the driver with STM32.
Could someone offer me a sample code of the driver to refer with any single chip such as MSP430.
And i can‘t…
Part Number: TLV2553 Other Parts Discussed in Thread: ADS8339 Hello,
I'm using a TLV2553 multi channel ADC. The output pins (data out and EOC) are connected to an analog devices level shifter P/N: ADG3304
For some reason the output pins will not drop…
Part Number: TLV2553 I have a few questions about the behavior of the device in shutdown mode.
When the device is placed in software power off and then powered back on is only the first conversion invalid?
When the device is in auto power off and powered…
Part Number: TXS0108E-Q1 Other Parts Discussed in Thread: TLV2553 , , SN74LVC2T45 , SN74LVC1T45 Hello
I use TXS0108E-Q1 to finish spi communication between 3.3V and 5 V for driving ADC TLV2553
THis is my Schematic:
I have read the reference book :the maximum…
Part Number: TLV2553 I am using the TLV2553 with a 400KHz data clock in a burst mode. I note the data sheet asks for a minimum hold of 0ns after the last falling edge of the clock. What would be the impact of a hold of -8.95 ns?
Thanks