Other Parts Discussed in Thread: TLV2772 , TLV2771 Hello All,
I'm trying to make a PCB for a charge amplifier of a piezoelectric device using the circuit shown below. However, I'm using 1x TLV2771 (for buffering the 1/2VCC) and 2x TLV2772 (I'm using 4 piezoelectric…
Part Number: TLV4112 Other Parts Discussed in Thread: TLV2772 , TLV4111 , , TINA-TI , LM7332 , UA741 Purchased 2 of these TLV4112CP for a new design because the TLV2772CP could not drive my load. MY design worked fine with the TLV2772 as long as the load was…
Part Number: TLV2772A-EP Other Parts Discussed in Thread: TLV2772 Hello. I have several questions regarding the datasheet/specifications for the TLV2772 opamp. All question apply to a simple voltage follower configuration (IN- tied directly to OUT) 1) What…
Hi Sanjeev:
Thanks for your reply.
Why does the TLV2772 has no issue , because of the different output structure ?
For the solution 1, do you mean the 1kohm pull down resistor on the output ?
For the solution 2, i didn't find theTLV316 has the shutdown…
Hi Gautam,
Can you tell me what is the input at pin4 of TLV2772 Op amp and where does this 1.65V come from ? What is and why we are using there 1.65V?
thank you
-Rahul
Other Parts Discussed in Thread: TLV2772 Dear all, i'm testing a 2nd order MFB Filter based on TLV2772 to Filter the 16/17KHz band of an audio signal.
The topology use 2,7v single supply with 1opamp for half biais voltage of thé 2nd opamp MFB Filter…
Other Parts Discussed in Thread: INA270 , TLV2772 Hi,
I am looking to use the INA270 in a design and wanted to carry out some simulations, the IC seems fairly straight forward to use, but the simulations will help show the process of design for my course…
Hi Gautam,
I was confused.
TS2640N321E64 Resolver, the specs for the t ransformation ratio is 0.5.
If the input of the resolver primary is 0~10V (sine wave), the output of the resolver would be 0~5V(sine wave). The hardware TLV2772 performs the 1.65V level…
Chris,
Thank you for quick response.
Also, I was wondering if the output range of the resolver in this paper (spry212) is -1.65~1.65V sine/cos wave? (because the hardware TLV2772 performs the 1.65V level shifting to meet the 3.3-V A/D input range.)
In…