Part Number: TLV316-Q1 Hi all,
What should be the linear full scale range input for TLV316-Q1 ?
I'm planning to use this Op-amp for high voltage measurement and so, I'm confused on understanding the minimum input voltage that should be provided at the…
Part Number: TLV316-Q1 Hi all,
What is the purpose of resistor 100K connected to 3.3V supply as shown in the schematic below. How to decide the value for that resistor ?
Please consider this query ASAP.
Thank You
Part Number: TLV316 Hi,
I am using TLV316 in differential opamp configuration with a gain of 2V. I wanted to know how can i measure the input offset voltage of the spice model of this part in pspice? Also how can I nullify this internal offset & how can…
Part Number: TLV316-Q1 Hi Expert,
Nice to talk with you. TLV316QDBVRQ1 will mass production on customer side.
Could you provide the Functional Safety FIT Rate, FMD and Pin FMA for TLV316-Q1?
If you need NDA to share this document, please send email to…
Part Number: TLV316 Other Parts Discussed in Thread: TLV9061 The datasheet for the TLV316 only lists a "typical" value of 10 MHz for the gain-bandwidth product. I measured this parameter on several parts and got values of around 2.5 MHz (see…
Part Number: TLV9001 Dear Team,
I use the TLV9001IDBVR in a circuit.
Unfortunately there is no availability for this part currently and it has a long lead time.
So I consider TLV316QDBVTQ1 for replacement.
Could you check TLV316QDBVTQ1 can replace TLV…
Part Number: TLV316-Q1 Other Parts Discussed in Thread: TLV316 , OPA316 , OPA657 , OPA656 , OPA838 , OPA837 Hi team,
Could you please provide what is the maximum TLV316-Q1 input offset drift? Datasheet only specified the typical value.
Thanks.
Best Regards…
Part Number: TLV316 Good morning,
i would like to use TLV316 opamp as comparator instead of finding for a comparator with push-pull output. My supply voltage is 5V, my input common mode voltage range is between 0V and 4V and the required output is about…
Part Number: TLV316 Other Parts Discussed in Thread: TINA-TI HI,
I am facing problem in spice model,
Its getting stuck at 52% and not moving further.
If i stop the simulation i am getting the error as Pspice_errors.docx
Part Number: TLV316 Other Parts Discussed in Thread: TLV9061 , TLV313-Q1 Hi,
I have the interest about TLV316-Q1. Do you have a release plan of DCK package? I want a small package with a lead frame.
Regards,
Y.Hashimoto