Part Number: TLV3202-Q1 Other Parts Discussed in Thread: TLV3202 How to design TLV3202 with ac hysteresis ? Are there any reference documents available ?
Part Number: TLV3202
Hello experts, I have question about equation (4) in datasheet P14. "Vin1 = R1 x Vref / R2 x Vref" is correct equation? It should be "Vin1 = R1 x Vref / R2 + Vref "? Thanks and best regards, Ryo Akashi
Part Number: TLV3202 Hi Team,
I understand TVL3202's Vcm is Vee-200mV to Vcc+200mV. Our customer intends to use single supply (+5V Vcc and 0V Vee), and have TLV3202 in a window comparator configuration detecting voltages outside the range of 0-5V.…
Part Number: TLV3202 Other Parts Discussed in Thread: TLV3201
Hi,
I am doing the simulation with TLV3201.
IN+: Pulse signal with 2MHz
IN-: Vref at 2.5V
Following hysteresis setting on datasheet Figure 29.
The output result is giving unexpected output…
Part Number: TLV3202-Q1 Other Parts Discussed in Thread: TINA-TI Jose Maroto Could you please support on this request ?
Need unencrypted Model for TLV3202AQDGK*Q1
Thank you,
Othmane
Part Number: TLV3202-Q1 Other Parts Discussed in Thread: TLV3202 , TLV9032 , TLV7032 , LM393LV
Hi
below is the circuit, during test, TLV3202 is easy to be damaged, mainly focus on pin 3, when pin 7 output 5V, pin 3 is 1.69V or 3.72V, it is 5V for good board…
Part Number: TLV9062 Other Parts Discussed in Thread: TLV9061 i want to simulate the TLV9062 OP AMP with 3.3v I did not find this model in pspice could u please suggest these model
Part Number: TLV3202-Q1 Other Parts Discussed in Thread: TLV3202 Hi team,
I have an issue in using TLV3202 as a comparator. While testing I supply Non inverting input (IN+) with frequency signal of 50% duty (Typically fat Low - 0V to High-3.3V levels)…
Part Number: TLV3202-Q1 Other Parts Discussed in Thread: TLV3201-Q1 , Hello,
I have two questions on propagation delay time specs of TLV3201-Q1 or TLV3202-Q1.
TLV3201-Q1 or TLV3202-Q1's data sheet specifies its propagation delay times, t PD , but what…