Part Number: TLV320ADC3101EVM-K Hi,
We are using TLV320ADC3101EVM-K in our solution. Please find below questions on same:
1) What is the maximum input impedance that can be interfaced to single ended input of ADC. as we would like to connect a low pass…
Part Number: TLV320ADC3101EVM-K HI,
We are using TLV320ADC3101EVM-K in one of our projects, we are trying to configure PCM and TDM modes from the TI GUI but unlike other protocols we don't find an option to configure PCM/TDM protocols. Could you please…
Part Number: TLV320ADC3101EVM-K Hi,
We are using TLV320ADC3101EVM-K, in our application.
As a initial testing, we have given 1V P-P as input to Analog input of Eval board (i.e. J6) and removed the W4 jumper. And we have connected the I2S output from J5…
Part Number: TLV320ADC3101EVM-K I have connected a TLV320ADC3101EVM-K via USB to a PC and it is not being detected by the ADC3101 CS software. Here's a screenshot:
In Device Manager, the eval board shows up like this:
I have installed and re-installed…
Part Number: TLV320ADC3101EVM-K Hello I just bought your kit but I can't use it. I am on windows 11 pro.
I installed the software, I changed the compatibility to windows 7 and when I run it as administrator it works but my card is not connected. However…
Part Number: TLV320ADC3101EVM-K Hi Team,
I have applied the ADC3101EVM and found that we don't provide the USB cable. Where can I apply the USB cable? The USB cable is the type B after checking the user guide. Can you show how to connect the EVM and PC…
Part Number: TLV320ADC3101EVM-K
Hi Guys,
I am getting the following message when I am running ADC3101 Control Software (CS).
I've installed the latest LabView runtime engine and still the SW does not start.
Please HELP
Part Number: TLV320ADC3101EVM-K
Hello ,
I tried the steps in the word file and still I was unable to fix the problem. Getting error Download command failed.
When I m connecting the EVM USB,
W11 disconnected
J6 1 and 3 connected
SW2 = A2 and external…
Part Number: TLV320ADC3101EVM-K Dear expert,
the PPS process flow do not work after upgrading the sampling frequency from 24K to 22.05K, it seems like the dsp register do not write successfully, the time waveform is not correct as expected in the process…