Part Number: TLV320AIC23B Hello,
Customer is a little confused by the note under table in 3.3.2.1 regarding the actual sample frequency capability of the TLV320AIC23B. According to this note, it looks like it means even if he configured 8KHz
sample rate…
Part Number: TLV320AIC23B Hi,
Good Day. I have a customer who is working with TLV320AIC23B. Please see below his query for your reference. Thank you very much.
I am using a TLV320AIC23B stereo CODEC as a slave, giving it BCLK, LRCLK, MCLK, programming…
Part Number: TLV320AIC23B Hi,
I tried to enable bypass mode in TLV320AIC23B but not able to hear anything on LOUT and ROUT.
Below is my procedure to enable bypass mode:
Reset Register : 0x00
Left line input channel volume control : 0x17
Right line input…
Part Number: TLV320AIC23B-Q1 Hi team,
I would like to know the clock configuration of TLV320AIC23B-Q1 at slave mode.
1. Is it possible to use Xtal instead of external clock input from MCLK in slave mode?
2. If yes, could you advise the requirement for…
Part Number: TLV320AIC23B Hi, Good day. Our customer wants to know if we have a device that is similar to TLV320AIC23B but with higher resolution (more than16bit, maybe 24bit). Because they are worried that the accuracy is not enough. The function of…
Part Number: TLV320AIC23B The data sheet for the TLV320AIC23B says on page 1-1, "Data-transfer word lengths of 16, 20, 24, and 32 bits, with sample rates from 8 kHz to 96 kHz, are supported." I am wondering what the resolution of the ADC and…
Hi GUO,
The TLV320AIC23B Data Manul, section 3.1.1 shows the SPI interface. With a typical MCU, the /CS is active while the SDIN is being transmitted and SCLK is typically 'off' while /CS is high. Please take a look at FIgure 3-1.
Part Number: TLV320AIC23B
Hi Team,
Customer R&D need to know TLV320AIC23B can replace ADI ADAU1761? and what difference between TAS2521 and TLV320AIC23B mini DSP function?
Part Number: TLV320AIC23B Hi
I am working on a project containing tms320vc5410 and the tlv320aic23b codec.
We have a bug with our DSP software.
Right after power up the first control word transmitting by the
DSP contains 15 clocks instead of 16 (Mcbsp…
Part Number: TLV320AIC23B Hi sir,
A customer want to know ho to deal with the pin1 IDENTIFIER metal.
Floating or connect to GND.
I can not find pin1 IDENTIFIER pad in PCB layout.
However customer want to know if there is an official suggestion how to connect…