Part Number: TLV320AIC3110 Hi TI team,
Customers use TI's TLV320AIC3110 chip in their distributed products, which can meet the audio recording, playback and loop out functions. Our test found that after the microphone distance from the sound source…
Part Number: TLV320AIC3110 Hello,
I am having an issue with the tlv320aic3110 codec. I get these two errors during boot up in my embedded device:
[ 10.079068] tlv320aic31xx-codec 0-0018: Unable to sync registers 0x1d-0x1d. -6
[ 10.161668] tlv320aic31xx…
Part Number: TLV320AIC3110
After powering on, writing to this register will produce a pop sound once. Is there any way to solve this problem? Thank you
The register configuration is as follows
P0_R4、P 0_R5、P0_R6、P0_R7、P0_R8、P0_R11、P0_R12、P0_R13、P0_R…
Part Number: TLV320AIC3110 Hi.
We are now facing codec white noise issue from line-out, except layout/placment and discrete components following, we would like to know any possible register finetune from codec itself? which one and where?
Or can you see…
Part Number: TLV320AIC3110 Hi,
We are using TLV320AIC3110IRHBR in our design for I2S interface. In datasheet it is mentioned as stereo Class D speaker. What type of speakers need to be connected. Is the mentioned speaker part number "AS01808MR-R" can…
Part Number: TLV320AIC3110 Hi,
We are using TLV320AIC3110IRHBR Audio Codec in our design for I2S interface. We would like to know the specifications for choosing the speaker. In datasheet it is given as 1.29W speaker, can we choose the speaker below 1…
Part Number: TLV320AIC3110 Hello,
I am using the tlv320aic31xx codec in my embedded device and I've noticed that, after forcing the unit into sleep and then, resume, I get a bunch of these errors: tlv320aic31xx-codec 0-0018: ASoC: error at snd_soc_component_update_bits…
Part Number: TLV320AIC3110
Hello,
I'm trying to limit the maximum volume level allowed for the tlv320aic3110. In our initial tests, when the volume is at its maximum default volume, it ends up damaging the speaker. For now, we are lowering the default…