Part Number: TLV320AIC3120EVM-U Loading filter coefficients from Pure Path into a TLV320AIC3120EVM-U via USB from a Windows PC. (Download and Run in the Build menu). The module, which was passing audio at the time, stopped communicating with the PC and…
Part Number: TLV320AIC3120EVM-U Hi
I am having issue with TLV320AIC3120EVM-U, software communication. The Leds on the board illuminate, but I get communication error from the the CodecControl.exe in slac366a.
I have went through forums and it seems this…
Part Number: TLV320AIC3120EVM-U
I have installed slac366, i.e. CodecControl on a Win 10 pro machine on english language. Connecting the EVM I get the message:
The evm is detected by windows as an audio device "usb miniEVM" (which doesnt work, but no…
Part Number: TLV320AIC3120EVM-U Hi,
I'm back on this project. I put a sine wave through my EVM and measured the BTL on both sides of the speaker through a low pass filter. I am playing the tone through this 4 ohm speaker: https://products.owolff.com…
Part Number: TLV320AIC3120EVM-U Other Parts Discussed in Thread: TLV320AIC3120 Hello,
We have a working prototype using this part. All of the clocking settings are unchanged from how the default init script on the EVM sets them. We are driving this speaker…
Part Number: TLV320AIC3120EVM-U Other Parts Discussed in Thread: TLV320AIC3120 I am planning to use the TLV320AIC3120 for audio input and output.
I'm trying to apply it to RF equipment, and I need to measure the output audio characteristics.
The…
Part Number: TLV320AIC3120EVM-U Hello
I've been working on using a host processor to set the registers how I want them. I have a very simple setup using a RaspberryPi Zero W as my host. I'm using the python interpreter and writing some basic settings…
Part Number: TLV320AIC3120EVM-U Other Parts Discussed in Thread: TLV320AIC3120 Hello,
I'm evaluating the TLV320AIC3120 for a voice amp application. I'm writing 0x10 to register 0x1D (Decimal 29) to enable ADC to DAC loopback. This works - I can…
Part Number: TLV320AIC3120EVM-U Other Parts Discussed in Thread: TLV320AIC3120 Hello,
We're wondering how best to implement a production-ready solution for our configuration of this part. The CodecControl GUI wants to write data to the EEPROM through…
Part Number: TLV320AIC3120EVM-U Other Parts Discussed in Thread: TLV320AIC3120
When connected via USB, the audio device driver is connected.
However, the program and board are not connected.
With PC to EVM, I2S data is connected. (Waveform check MCLK…