Part Number: TLV320AIC32 Other Parts Discussed in Thread: TLV320AIC3105 , HI,
I'm trying to use tlv320aic32irhb audio codec chip,(note not evm).
1) how can i connect to pc to configure internal gains of adc and dac etc? is there some uart method to do…
Part Number: TLV320AIC32 Hi,
One of my buyer request the audio impedance data.
I cannot find from TLV320AIC32 datasheet, so please let me know.
input/output is used as mono.
input : Pin10 (MIC1L/LINE1L)
output : Pin27 (LEFT_LOP)
thanks,
TS
Other Parts Discussed in Thread: TLV320AIC32 Hello,
I have some problem with routing LINE2 R/L to output amplifier.
My application is to use codec as audio mixing matrix (without I2S at all).
According to datasheet, LINE2 can be routed to output drivers…
Other Parts Discussed in Thread: TLV320AIC32 Is there any code available for an I2C driver to configure the TLV320AIC32 ? I am using a Microchip dsPIC33EP512MU810 but I2C is new to me so I am finding it difficult..
I have a WT32i bluetooth development…
Other Parts Discussed in Thread: TLV320AIC32 , TLV320DAC3100 , TLV320AIC3100 I am looking for an alternative replacement for the TLV320AIC32 that has a more powerful headphone amplifier (~2W).
The replacement needs to have an I2S audio input digital interface…
Other Parts Discussed in Thread: TLV320AIC32 I am using a TLV320AIC32 which has the differential line outputs connected to an external amplifier TPA6120A2DWP.
Originally I had the TLV320AIC32 configured to use the headphone outputs, but now I would like use…
Other Parts Discussed in Thread: TLV320AIC32 Hi, guys,
We are using TLV320AIC32 on our board, which have pop and click problem , we are using LINE1L and LINE1R as analog input and LEFT_LOP AND RIGHT_LOP as analog output and also DOUT/WCLK/BCLK as digital…
Other Parts Discussed in Thread: TLV320AIC32 The manual for the TLV320AIC32 states that after the power supplys are good, the RESET must be driven low for at least 10ns. Taken literary, that would mean that the RESET has a falling edge, then a rising edge…
Other Parts Discussed in Thread: TLV320AIC32 Hi, All
I am using TLV320AIC32 codec with DKWT32i-A Bluegiga kit. I want to generate some filters of EQ mode, like JAZZ, ROCK, BASS. and etc., but I can't.
The communication between BTI module and TLV320…
Hello,
I want to connect the TLV320AIC32 on a raspberry PI. The raspberry PI have a PCM interface (on the connector P5).
My question is how to connect MCLK, BCLK, WCLK, DIN and DOUT on the PCM interface of the raspberry (PCM_CLK, PCM_FS, PCM_DIN and PCM_DOUT…