Part Number: TLV320AIC3268 Other Parts Discussed in Thread: TLV320AIC3262 , Hello everyone,
i based my design around the TLV320AIC3262 and make some test with the dedicated EVM but i'm realizing that the BGA 0.5mm pitch is little bit more difficult to implement…
Part Number: TLV320AIC3268
Hello Everyone,
i'm playing with the miniDSP of the TLV320AIC3268.
we're porting our job from 3262 (and we have good experience with 3254, so Purepath and TLV are not new for us).
we created this flow (to make test…
Part Number: TLV320AIC3268 Hello everyone,
Does the pins SVDD, SPK_V and RECVDD_33 has to be powerered even if REC and SPK output are not used ?
thank you
Sebastien
Part Number: TLV320AIC3268 Hello everyone,
i couldn't find the common Application Reference Guide on TI website for the Audio Codec TLV320AIC3268.
do you know if this file is available ?
thank you
Sebastien
Part Number: TLV320AIC3268 Other Parts Discussed in Thread: DRV601 , Hello TI member,
I would like to use TLV320AIC3268 CODEC with DRV601 line driver. The block diagram shown as below:
My questions are as follows:
1. Can I use the RECP-RECM pins of the TLV320AIC3268…
Part Number: TLV320AIC3268 Hi
There two questions about TLV320AIC3268
1. How long does RESET pin pull down to enable reset? and How long does I2S clock need to be maintained before entering the software configuration?
2. Is there any register that can…
Part Number: TLV320AIC3268 HI Team
I afraid of missing some device that I don't know, so I would like to double check with you on the DSP devices which can support Dolby Atmos.
Thank you!
Joe
5 Dec
Part Number: TLV320AIC3262 Other Parts Discussed in Thread: TLV320AIC3268 , PUREPATHSTUDIO Hi, TI
For a new design, we are considering using the TLV320AIC3262 or TLV320AIC3268 codec. I read conflicting information about anti echo on mini dsp. I do not yet…
Part Number: TLV320AIC3268 Dear Sir,
I have a sound bar system that has (I2S-IN) header. The signals present on these headers are (LRCLK, BCLK, MCLK, and Data0-Data3). Of course HDMI eARC host(TV) side connector(19 pins) is sending audio signals to reciever…
Part Number: TLV320AIC3268 Dear team,
Do we have suitable solution can meet below spec?
This case only needs the input/output two-channel audio codec for the amplifier application, and the design will need to use 2 sets of I2S, if the price is competitive…