Part Number: TLV320DAC3203EVM-K Hi Ivan,
I am again working on a script with Adaptive Filtering, using the EVM as start point.
While checking everything, I discovered the following lines on the command interface:
(this will be added to the command interface…
Part Number: TLV320DAC3203EVM-K Other Parts Discussed in Thread: TLV320DAC3203 Hi Ivan,
going on with the settings of the TLV320DAC3203, I am now testing with a higher MCLK.
I read in the Reference Guide (slau434a), by the settings for Fast Startup: "The…
Part Number: TLV320DAC3203EVM-K Hi dear people!
Sorry, I need more explanations or help. The example presets on the GUI are for 44.1kHz use. I would like to work with 48kHz and with a rather low MCLK frequency of 2.048MHz. (This is the frequency coming from…
Part Number: TLV320DAC3203EVM-K Other Parts Discussed in Thread: TLV320DAC3203 Hi dear people,
continuing with my project using the TLV320DAC3203, I have some questions related to MICBIAS settings:
On the TLV320DAC3203 Applications Reference Guide I can…
Part Number: TLV320DAC3203EVM-K Hello.
I am having trouble starting the GUI for the TLV320DAC3203EVM-K.
I selected "Run as administrator" and started the TLV320DAC3203EVM-K_CS.exe, but it says "The LabVIEW RunTime engine could not be found." is displayed…
Part Number: TLV320DAC3203EVM-K Other Parts Discussed in Thread: TLV320DAC3203 Hello,
Our customer is running TLV320DAC3203EVM-K.
It works fine with Fs 44.1KHz USB audio source, but if change FW setting for Fs 48KHz as following the procedure on GUI then…
Part Number: TLV320DAC3203EVM-K Other Parts Discussed in Thread: TLV320DAC3203 Hi Ivan,
I am back here with the question about shut-down of the TLV320DAC3203.
It is said in SLAU434A:
The DAC Modulator is clocked by DAC_MOD_CLK. For proper power-up of the…
Part Number: TLV320DAC3203EVM-K Other Parts Discussed in Thread: TLV320DAC3203 Hi dear people,
I am having troble to operate the TLV320DAC3203EVM-K.
Basically, I have the same issues as in the following post: https://e2e.ti.com/support/audio-group/audio…
Part Number: TLV320DAC3203EVM-K Am I correct that to apply a external MCLK clock to P22-17 on the EVM board that on the USB-MODEMEVM board, SW2-5 must be OFF and SW-2-8 must be on?
When I set the switches this way, I notice that applying an external MCLK…
Part Number: TLV320DAC3203EVM-K Using TLV320DAC3203EVM-K connected to the USB-MODEVM, I can setup the device using I2C
P12-20 SDA
P12-18 Ground
P12-16 SCL
and it functions correctly. If I disconnect the USB-MODEVM and add the connections as follows:
…