Part Number: OPA569 Other Parts Discussed in Thread: OPA548 , , TLV4110 , TLV4111 , OPA2677 Hi Team,
Our customer is looking for a voltage follower with current sink capability of 150mA that will be driven by a single 5V supply voltage, has an input voltage…
Part Number: TLV4113 Other Parts Discussed in Thread: TLV4111 , TLV4110 When driving a 10 Ohm resistor on the output of the TLV4113 with a 1V output for 100 mA current. The input of the OpAmp was stable while the SHDN# was pulled high.
We note about 200µs…
Hi Mark,
Thanks for the further insight into your 200 mA application.
The OPA551 power op amp is rated for a 200 mA continuous dc output current. Its unity gain bandwidth is typically 3 MHz and is intended for lower frequency applications. Its supply…
Other Parts Discussed in Thread: TLV4110 , TLV4112 , TLV4111 Hi,
My requirement is that I need to accept a signal between 1-100 KHz, and supply it on 6 output ports. In short, I am looking for a 1-to-6, or at least 1-to-2 analog output drive buffer. Can…
Hi Faisal,
You didn't mention the supply voltage you would be using, but if it is something on the order of 2.7 to 5.5 V take a look at the TLV4110. It is a CMOS, single-supply operational amplifier that can sink/source up to 300 mA. The data sheet can…
Okui-san,
The next step up in higher output current would be the TLV4112. The TLV411x family is capable of output currents in excess of 300 mA, with V+ of 5 V. The power and thermal considerations in data sheet pages 13 to 16 must be carefully observed…
Thks Marek for your fast answer.
I have been using TLV4110 as a regulator to supply MSP430. At the input of MSP430 I have 2 caps: 10uF//100nF, and the MSP430 may draw a current of up to 100mA.
I set the amplification factor of the TLV4110 to 2. Its…
Other Parts Discussed in Thread: TLV4110 , OPA569 I am trying to design an inexpensive solar cell current-voltage tester for educational modules related to solar energy. The purpose of the circuit is to sweep an applied voltage across a solar cell and measure…
Other Parts Discussed in Thread: BQ25504 , TLV4110 Hello all,
I am looking for a device which converts from (0-20 )mV dc input to (0-5) V dc output voltage with higher accuracy.
Like below..
0 mV -- --------> 0 V 10 m V----------> 2.5 V 20 mV----…