Part Number: TLV521 Dears,
Just curious what's the purpose for adding a transistor in the sensing circuit? Generally, without the transistor, just use an op-amps could monitor the current.
Hugh
Hi both,
yes, such a statistical approach may be reasonable for many cases. But for a professional product you will need maximum specifications. We sell a product with a board containing more than 30 OPAmps (all from TI by the way ). If only one OPAmp…
Part Number: TLV521 Other Parts Discussed in Thread: OPA355 , THS4631 Hi Team, I would like to get your suggestion for the customer request below as I am lacking in seeing the slew rate information in other datasheet for the complete requirement of our customer…
Part Number: TLV521 Team, customer plans to use TLV521 op amp in thier design as a buffer for a voltage reference. As such, they plan to use it as unity gain follower with a 10μF filter capacitor. Their question is: What value of isolation resistor I…
Part Number: TLV521 Have attached a ckt, basically its a low pass filter of 240Hz & then high pass filter of 10Hz. Can someone tell why output of HFP filter is getting clipped. Is it due to capacitive load? If yes how to solve it?
Otherwise CMR range…
Part Number: TLV521 Other Parts Discussed in Thread: TLV7031 Hello,
My customer needs to know if the absolute value reported in the ds (300mV) (PAGE 2 PARAGRAPH 6) for Differential Input Voltage can be greater or not.
Customer realized that under certain…
Part Number: TLV521 Dear, Sir.
My customer is considering to apply TLV521 for their system, now.
The circuit is similar as Figure34 on the datasheet(using single power supply).
They are concerning the negative voltage around -0.3V on IN+ pin will be…
Part Number: TLV521 Hi.
I tried to find the input resistance and capacitance value of TLV521 on its datasheet, but thers is no informations about this.
So, I wonder the input resistance and capacitance value of TLV521 amplifier.
Is there are any informations…