Part Number: TLV62130 Hi team,
Customer is checking the package size with us, could you help provide the spec of the marked corner place?
Thanks and Best Regards,
Will
Part Number: TLV62130 Hi Team,
currently we are using TLV62130 part. As per our application there will be a voltage generated on the Vout pin when there is no vin. We just want to confirm whether the diode present internally is reverse path blocking supported…
Part Number: TLV62130 Other Parts Discussed in Thread: TPS62110 Hi TIer
Do we have a chip which pin2pin TLV62130 and its output voltage include 7V?
Customer want to find a chip like this. I do not find it on Ti .COM.
I think the current advanced technology…
Part Number: TLV62130 Hi team
We are using TLV62130RGTR in our product, we have requirement to use 2 9V battery (9V MN1604 / Size: 9V (6LP3146) ) in series it will become 18V. Is it safe to use 18V since max recommended 17V ??
Thanks and best regar…
Part Number: TLV62130 Hi I use TLV62130RGTR to generate 1.8V and 1.0V power as picture 1 and picture 2 show. there two schematic are the same.
for 1.0V power, it works normally.
for 1.8V power, it does not work.
for 1.8V power, what i did as below
1)…
Hi Sangil,
After looking at your schematics and layout again:
1) Where is the RESET_OUT_L signal going to in your schematic? Is there a pullup resistor?
2) There is a lot of ringing on the SW node which could be due to measurement technique and layout…
Part Number: TLV62130 Other Parts Discussed in Thread: TPS61253A , TPS62933O Hi, Team
My customer is looking for a Buck DCDC, Vin 20-25V, Iout:2-3A, Vout:5V
But since the project is use in portable smart speaker with 2 cells battery, they prefer the DCDC…
Part Number: TLV62130 We've been using TLV62130 for many years now in multiple devices, not giving problems.
The protoboards of our latest devices all worked fine.
Validation of the final PCB was done, all OK.
Now after putting the first batch of …
Part Number: TLV62130 What is the behavior of the TLV62130 under the following conditions / What output showed under following condition:
a) When Input capacitor between PVIN to PGND is short circuit?
b) When R2 (on FB pin) is short circuit?
Assume that…
Part Number: TLV62130 Other Parts Discussed in Thread: TPS62903 On another device that returned 'dead', we noticed again a low voltage on the EN pin: 0.48V when pulled up to Vin@5.0V over a 1K resistor. This indicates a much higher current than…