Part Number: AMC3301EVM
We are still learning what the problems are.
Firstly, we were getting spurious noise on our AC shunt measurements on some of the boards. After investigating more, we think this is occurring on the 2 pin boards, but we are not…
Part Number: AM2634
Environment
HW: AM263x_launchpad_EVK
CCS Version: 12.5.0.00007
FreeRTOS
Question
I am working on an existing FreeRTOS, which uses heap 4 scheme in the FreeRTOS. I need an idea whether CCS needs the user to enable compilation of a…
Hi Ayush,
Thanks for your patience as I have been out of office traveling.
Can you confirm the following:
What operating mode are you in (Register 0x12)?
What is your port power allocation (Register 0x29) prior to turning on the ports?
Please confirm…
In this situation, if I set MPU as no access to unused flash region, CPU can't fetch any instruction from unused flash region. Normally, CPU generates an abort but there isn't an error because of discarding this operation. Also ESM 2.3 error doesn't recieve…
Part Number: DP83822H Hello expert,
May we know if you can provide MIIM 1 to 2 buffer, 3 channel solution to my customer? Thanks a lot!
Best regards,
Ann Lien
Hello Amy,
To which 960 RX port is the 953 connected?
Are you switching from Mode #2 to #3 or the opposite?
Are you making any register changes on the 953 when you are making this switch? You need to make some changes in reg 0x05
can you provide register…
Part Number: LP87745-Q1 Hello,
we use the LP877451A1RXVRQ1 with a switching frequency of 17,6MHz set by OTP.
Is there any way to change the switching frequency to 8,8 MHz by software,
or we need a new OTP version?
Best Regards