Part Number: TLV7031 In application note SVNA808 a circui is depicted showing the TLV7031 with an IR LED although it is used as a photodiode.
The circuit does not work with normal photodiodes because they produce such a high photocurrent that the voltage…
Part Number: TLV7031 I have a pull up of 10k Ohm at the positive input pin and a pull up of 470 Ohms at - negative input pin. I am using only +5V power supply. I am getting low ( zero volts) at the output. Is it possible that the output becomes high for…
Other Parts Discussed in Thread: PSPICE-FOR-TI , TLV7031 Hello, Excuse me in Japanese.
日本語で恐縮です。
技術ドキュメント「JAJA598–July 2018」と同じ回路で PSPICE-FOR-TI を使用してヒステリシスの検証を行おうとしています。
シミュレーションは、TLV7031デバイスのページから 「TLV7031 PSpice Model (Rev. A) SLVMDG0A.ZIP (44 KB…
Part Number: TLV7031 Good morning, I am having some trouble with a comparator circuit I've designed on a IO breakout board that I'm hoping I can get some help with. The circuit in question is the front end to a fan circuit. The purpose of the comparator…
Part Number: TLV7031-Q1 Hi Team,
I'm also having the same issue:
is it allowed if the supply voltage of the TLV7031-Q1 (5V) is turned off and there is still a voltage at the in+ and in- inputs (e.g. 3V) for a long time ?
but the TLV7031-Q1 should not…
Part Number: TLV7031 Other Parts Discussed in Thread: TLV9032 , TLV1805 , TPS1663
Hello everyone, I am designing a typical electronic fuse (unfortunately I cannot find an eFuse that opens the circuit with 11A) I have already designed all the stages, but…
Part Number: TLV7031 Other Parts Discussed in Thread: STRIKE We have a comparator that we use for a input detection and I would like to discuss on a call how to protect the input or if we need to. We have a divider that goes into the the positive input and…
Part Number: TLV7031TLV7031: Zero crossing detection is not at 50% duty cycle - Amplifiers forum - Amplifiers - TI E2E support forums
The simulation circuit mentioned with the capacitor doesn't seem to simulate in tina, it Stucks in the middle. Can…
Part Number: TLV7031-Q1 Hello, Team,
Could you check whether below circuit is OK?:
*コンパレータ = Comparator
Comparator inputs are: - Lo -> Hi @ 2.64V, Hi->Lo @ 1.65V
*Green = Input, Blue: Output
Please note that green is actually a pulse but represented…