There are current-sense amplifiers with a (latching) alert output like the INA381 or INA300. But you probably do not need their differential inputs, and their minimum amplification might be too high.
Alternatively, build a set/reset latch from two NAND…
Part Number: TLV7031 Hi Team,
Could you please tell me how I/P signal frequency and comparator delay is related.
When I used nanopower comparator my i/p and o/p are out of phase.
https://e2e.ti.com/support/amplifiers/f/14/t/833681
Regards
hari
Part Number: TLV7031 Other Parts Discussed in Thread: LM7332 , TLV7011 Hi Team,
I tried to design a non-inverting comparator using TLV7031. My Vh is 3V and Vl is 2.4V and Hysteresis is 600mv.
Let me explain how I approach the problem. From the datasheet…
Part Number: TLV7031 Other Parts Discussed in Thread: TLV4021 , TLV3701 Hi,
is it allowed if the supply voltage of the TLV7031 (3.3V) is turned off and there is still a voltage at the in+ and in- inputs (e.g. 5V)?
it's no problem for me if the output…
Applying a voltage at the inputs while the power supply is off violates the absolute maximum ratings. (A current will flow through the input ESD protection diodes into V+.)
The purpose of the shutdown function is to allow the opamp to stay connected to…
Part Number: TPS61094 Other Parts Discussed in Thread: TLV7031 , LM334 , BQ25504 , , TPS61299 , TPS7A02 , TPS7A03 Hi there,
I am working on design that uses TPS61094 to regulate the output of BQ25504 to 4.5V to remove the effect of MPPT. The TPS61094 is loaded…
Part Number: TLV7031 On the suggested schematic, i would like to change the RC network so i can have a 1Hz pulse with 10-20msec duration.
I don't know how to calculate the resistor/capacitor values.. can you help me please?
Hi Dennis,
thank you very much!
Do you know if the same issue is persists here too? It's in the same application note, the voltage divider R3 and R5 output a voltage higher than 3.3 V when the voltage above is 24 V. According to the datasheet the…