Part Number: TLV7032 In the TLV7032 datasheet, we see in section 6.9, the Electrical Characteristics (Dual) table, that the minimum, maximum, and typical values are provided assuming certain test conditions. Many of these test conditions involve the TLV7032…
Part Number: TLV7032 hi team,
Once of our customer is currently evaluation TLV7032DSGR. Could you kindly have a quick look into below customer question(s) and help providing feedback?
I have some questions regarding the TLV7032DSGR, which could be a good…
Part Number: TLV7032 Other Parts Discussed in Thread: TLV7031 , , TLV1701 , TLV7041 Hi,
I'm trying to simulate a window comparator with the TLV7032. I have tried using both the TINA model for TLV7031 (x2) and the model linked in this previous question (…
Part Number: TLV7032 Hi team,
Do we have the simplis model or Tina model for TLV7032?
If don't, do we have similar device which have the model?
Customer needs this model to simulate a related circuit.
Thanks a lot for your help!
Part Number: TLV7032
Hi application specialists.
I am Yuki Japan TSR.
Could you tell me when dose TLV7032 relase?
Thank you for your kind help
Best regard
Yuki
Hi Sharu,
I see on the TLV7032 data sheet that IN+/- can be up to 100mV higher than V+/lower than V-.
It is similar on TLV1812 (rail-to-rail +/-200mV) and TLV1851 (IN+/- can be from -0.1V to 40V independent of V+).
If using TLV1851 (or another comparator…
Hi Chuck,
At this point, I believe I'm fine. I think I have come as far as I can, concerning simulations. If I wanted to simulate this, I would need to have it included in the SPICE data, since I would want to have a more realistic response for a power…
Other Parts Discussed in Thread: OPA2333P , TLV7031 , TLV7012 , TLV7011 , TLV7032 , TLV4051
Hi Sir,
My customer would like design OP with the following spec.
low Iq, like( less than 10uA per channel),
Vin is 5.5V max
Vin is 2.5V min
Push-pull or Open drain…
Part Number: TLV3202-Q1 Other Parts Discussed in Thread: TLV3202 , TLV9032 , TLV7032 , LM393LV
Hi
below is the circuit, during test, TLV3202 is easy to be damaged, mainly focus on pin 3, when pin 7 output 5V, pin 3 is 1.69V or 3.72V, it is 5V for good board…