Part Number: TLV705 Hi Sir,
Would you please helping to check which pitch is A1 at TLV70530YFMR? is A1 is at the blue square I draw at the fig? Thanks for your kindly help.
Best regards,
Gary Teng
Part Number: TLV705
Hi Experts,
I have this client who is having hard time identifying the pin numbering of our small LDO device, TLV70518YFMT.
At first, I am thinking that by looking at the surface of this device, showing a dot mark, would help him…
Part Number: TLV705 Hi Team,
1. Is there any measurement data or curve about Tj to output accuracy?
2. I found the most related curve is figure6 in datasheet, but does TI has the same curve in 3.6Vout?
3. If not, then how can I expect the deviation compare…
Part Number: TLV705 Hi Team,
According to Figure3., the accuracy is about 0.5% over temp., may I know what condition could make the output accuracy up to +/- 2%(from datasheet 6.5)?
Thank you very much.
Best regards,
C.T.
Part Number: TLV704 Other Parts Discussed in Thread: TLV705 Hi Team
Can you help to provide the thermal data of TLV705 at this set up: Vin=15V, Vout=3.3V@10mA in our EVM?
Hello,
There is no other device except DS90UB953 and its power supply circuit. The power chip uses TLV705 to provide 1.8V power, and the Sensor is at the far end and the connector is at the back.
Hi Expert,
My customer would like to know is there any side effect about Enable pin and Vin power sequence.
If EN pin signal is enable before Vin power source, is there any side effect ot is this not allowed?
Please advise.
Thanks
GPIO28 is connected to EN of this LDO which draws 10nA: https://www.ti.com/lit/ds/symlink/tlv705.pdf?HQS=TI-null-null-digikeymode-df-pf-null-wwe&ts=1600904541651
We're at 3.3V and there is a 100k pull down. That puts us at 33uA + 10nA. Too high…
Part Number: TPS7A10 Other Parts Discussed in Thread: TLV705 Hi Sir
May I know TPS7A10's height is 0.3mm or 0.4mm
Have any TI LDO solution the height is under 0.3mm?