Part Number: TLV757P Hi TI,
We use the SOT-23 package, our customer ask us , what's parameter do we use for calculation the thermal temperature?
If we measure the IC surface, what parameter do you suggest to calculate the junction temperature? Rjc…
Part Number: TLV757P Hi All,
Is the TLV757P available in a 1.35V output? The data sheet says it comes in fixed outputs from 0.6 to 5.0V in 50mV steps but I don't see an orderable. I have a customer who would be interested in the part in 500K EAU's so…
Part Number: TLV757P Hi Sir,
May I know if TLV757 can achieve 1.8V transform 1.2V?
(TLV757 dropout voltage is 1.2V, looks cannot support it.)
If not, do you have good part can do it?
Thanks, Ian.
Part Number: TLV757P Hello team!
Could you please tell me the current protection behavior about the device?
I read 7.3.3 on DS but not sure my understanding is correct or not.
For the short event, the current is limited by 755mA(typ).
For the…
Hi Hirotsugu,
Yes the thermal information for TLV757P listed in the datasheet matches our current thermal models for the device.
There are a variety of factors that impact the thermal performance of a device including leadframe, die size, die placement…
Part Number: TLV757P Other Parts Discussed in Thread: TINA-TI Hello,
I am attempting to create a TINA-TI model for the TLV75712P.
When I was attempting to add a new macro model in TINA-TI I received this error:
Redeclaration of identifier: D_D1…
Part Number: TLV757P Hello.
There is a problem when EN pin voltage is higher than IN voltage.
Briefly describing my system, VIN is lipo battery(3.0~4.2V), VEN is connected to Vbatt(3.0~4.2V) or external usb power(about 5.0V).
TLV75733 works well…
Part Number: TLV757P Hi,
During development of our product, I bought 10pcs of TLV75733 from Mouser november last year. But we are encountering issues on the 1000pcs that we bought directly from TI store.
2nd picture shows output from mouser batch…
Part Number: TLV757P Hello team,
Could you please tell me the max ambient/package temp for this device if your team has?
From my understanding, the junction temperature is dominant and those values would change depending on the junction temp.
…
Part Number: TLV757P Other Parts Discussed in Thread: TPS7A91 , TPS7A83A Hi TI Team,
We are using TLV757P component in our design,
Please find the attached schematic and review the same and share your valuable comments on this to improve the design…