Part Number: TLV760
I need to calculate the junction temperature of the TLV76012 component in my application. I have measured the temperature on package top with an IR camera, and it is 84 ºC at an ambient temperature of 20 ºC. The component dissipates…
Part Number: TLV760 Hi Team,
Could you please help to advise whether TI has done phase margin testing for the TLV760 LDO?
Phase margin testing method reference document "Ti_snoa507" as attached.
Ti_snoa507.pdf
Best regards,
Terry
Part Number: TLV760 Hi experts,
My customer is searching for LDO. Could you recommend suitable device? Thanks.
Vin:24V
Fixed vout: 12V and 15V
Actual load current: 90mA
Low cost
BR,
Victoria
Part Number: TLV760 Hi,
Could you please make the graph of Psi-JT vs " PCB copper coverage are such as Vdd/GND Size"?
The result of thermal on Package top is different from calculation with Psi-JT. My customer is thinking Thermal pad size such…
Part Number: TLV760 Other Parts Discussed in Thread: LM317 Can you stacking regulators to increase voltage (2 12V to create a 12V and 24V output for example) or can you raise the output level of the 12v using external resistors and which configuration…
Part Number: TLV760 I have a switching regulator ( LMQ61460AAS, 24V Input) with a variable output voltage (22V - 10V) and also need a fixed voltage of 3.3V (max 8mA). I chose the TLV760-33 for the 3.3V.
Currently I have connected the linear regulator to…
Part Number: TLV760 Other Parts Discussed in Thread: TPS7B69 , TPS709 Hi all,
I am looking for a replacement for the LM3480IM-15NOPB, where I have found the TLV76015DB. Can you help assist me in determining differences between the two parts?
www.ti.com/…
Part Number: TLV760 Hi team,
I would like to confirm about Figure 16 "Output Current vs Input Voltage".
It indicates "Vout(Red)=3.3V".
Is it correct to think that Red line shows max output current with various Vin condition from 5.8V…