Part Number: TLV767-Q1 Tool/software: Hi team,
My customer would like to improve the thermal dissipation performance of TLV767-Q1 by optimizing the PCB layout design. Are there any good materials to explain how to optimize the PCB layout design of LDO…
Part Number: TLV767-Q1 Other Parts Discussed in Thread: TLV767 Tool/software: Hi, TI expert
We have a request from a customer to review the PCB layout of TLV76701QWDRBRQ1.
Please review it to see if there are any issues.
TLV767-Q1_(PCB drawing)…
Part Number: TLV767-Q1 Tool/software: Hi, TI expert
A customer has requested a schematic review of the TLV76701QWDRBRQ1.
- Application : Local-Dimming of 17-inch LCD for Vehicles
- V_LED: 12.4V applied
- OUT Voltage: 6.8V
Q1) For C229, which…
Part Number: TLV767-Q1
Tool/software:
Hello,
I am considering using TLV767-Q1 for my project. I read through the datasheet and found that it has two variants, fixed-output voltage and variable output voltage. I need one with fixed 3.3V output voltage…
Part Number: TLV766-Q1 Other Parts Discussed in Thread: TLV767-Q1 , , TPS7B86-Q1 Hi team,
Customer is choosing LDO for transmission control unit and has high ambient temperature VIN=14V,VOUT=5V,Iout=150mA ; (Ta=115 ℃ );
I'm promoting TLV766-Q1 but…
Part Number: TLV767-Q1 Hi,
Can you Please provide the value of line regulation for Vin=6.5V (5% Tolerance) & Output current (550mA).
And also the value of Load Regulation For Output current 550mA( 5% tolerance).
Output voltage is 5V(2% Tolerance…
Part Number: TLV767-Q1 Hi,
Can you share the graph of Ground current VS Output current for Vin(Input voltage) = 6.5V. In the datasheet it is mentioned but for different Vin conditions. see the image
Regards,
Ajay
Part Number: TLV767-Q1 Hi,
Can you please tell what is the copper area for which the value of thermal resistance (junction to ambient) is 51.9 degC/W
Regards,
Ajay