Hi Micou,
I have not heard back from you. I suppose the issue with error connecting to the target is resolved. I will close this thread for now. You can update this post if there is any update and the thread will automatically reopen again.
Part Number: TM4C1230E6PM Hi,
I am using TM4C1230E6PM microcontroller, I want to save unsigned long number (4 Byte) information in memory, when power goes its will save this variable data in memory and when its Power ON, can retain this 4 byte value…
Part Number: TM4C1230E6PM Hi,
I have several systems that communicate through the CANbus. Microcontrollers use ADC, master I2C, CANbus and systick. all ms, an ADC measurement request is made and every 100ms, I read data on the I2C. the microcontroller…
Part Number: TM4C1230E6PM Hello,
I have the PBORCTL register which has not been modified (BOR0 and BOR1 to 1). When I changed the microphone voltage for what to 2.88V, I did not have a reset as indicated in the datasheet. Do you know why he doesn’t reset…
Part Number: TM4C1230E6PM Other Parts Discussed in Thread: BQ34Z100 Hello,
I have a tm4c1230e6pm who read a bq34z100-z1 gauge. when I have a big current disappearing, I can no longer communicate with the gauge. I have the signals below. I try to reset…
Part Number: TM4C1230E6PM Hello,
What is the typical/ expected pull up/ down resistor drive strength when configured as an input? I understand that these weak pull ups are different than the output drive settings and the datasheet doesn't specify a parameter…
Part Number: TM4C1230E6PM Hello,
I have a code with many error.
Description Resource Path Location Type #131 expected a "{" srv_tick.h /BOOT_BATEAU_TI/Sources/Srv line 21 C/C++ Problem #20 identifier "DELAY_ACTIVE" is undefined srv_tick…
Hi,
I have not heard back from you. I assume you have resolved the issue. I will close this thread for now. If there is any update from your side, simply write back to this post and the thread will reopen.
Part Number: TM4C1230E6PM Hi,
I have a question about ADC differential sampling.
My customer connected VIN+ to the analog input and VIN- to GND on board.
The board has an input voltage range from 0V to 3.3V.
When the input is 0V in differential mode…
Part Number: TM4C1230E6PM Hi TI Comunity,
I was wondering if you are able to point me to any materials or info about bootloaders for TM4C12xx family that would allow me to flash new firmware over CAN? Thank you Eryk