Part Number: TM4C1231D5PZ All,
This is more a question related to the Tiva peripheral library, when using ADCClockConfigSet, is it actually mandatory to provide any ADC_CLOCK_RATE_* argument?
Currently we call this function as "ADCClockConfigSet(ADC0_BASE…
Part Number: TM4C1231D5PZ Hi
Is the following a problem? We use 2,5V as VREFA+ while our VDDA is 3,3V.
The datasheet seems to say the minimum for VREFA+ is 2,4 and a typical is VDDA (which is minimum 2,97V).
In the driverlib code (TivaWare_C_Series-2.2…
Part Number: TM4C1231D5PZ Other Parts Discussed in Thread: EK-TM4C123GXL Hi all
I am trying to update my TM4C123 controller using I2C. Unfortunate, something goes wrong and I don't have a clue.
I follow the 5. Serial update for packet handling. Sending…
Part Number: TM4C1231D5PZ
Hi
I am facing some interrupt issues.
Using below code, does not trigger my interrupt function. (The button is pulled high and should go to 0 when pressed, this is confirmed using a scope)
If I change everything to do it polled…
Part Number: TM4C1231D5PZ
Hi
I am having some troubles using both ADC on the TM4C1231D5PZ. Both ADC seem to be configured correctly and pinmuxing seems ok as well. For some reason I am undable to read all channels. I am using channel 0 - 11 and 20. Channel…
Part Number: TM4C1231D5PZ Hi everyone....
I am using TIVA TM4C1231D5PZ and having problem with building target.
The error I am facing in this line "__STACK_TOP =__stack + 512;".in the linker file.
Name of Error is __stack is undefined.
Any help…
Part Number: TM4C1231D5PZ Hi,
We are using TM4C1231D5PZ for an RS485 based application.
The RS485 tranceiver operates at 5V and hence the receiver output is at 5V. Can we connect this signal directly to the UART_RXD pins of the controller?
Part Number: TM4C123GE6PM Other Parts Discussed in Thread: TM4C1231D5PZ
Hi
We created a custom board with a TM4C123GE6PM, but are unable to program the controller using JTAG. The JTAG used is the ICDI interface from a TM4C123 Launchpad. Previously we used…
Part Number: TM4C1231D5PZ Hi,
When I try to set the uC RTC seconds using Seconds_set(1569332907), it will pend. I found WRC bit in HIBCTL is never set.
Can you give us any clue?
Thanks,