Other Parts Discussed in Thread: TM4C1236E6PM Hello everyone,
I'm received a board with a TM4C1236E6PM microcontroller. It has a jtag interface brought to a connector. I've been trying to program it with my XDS100V2 but I get this error:
"…
Thanks for your reply Martin,
I'm using the TM4C1236E6PM. The spi clock frequency is 6.1MHz. The CHIP_RDYn is indicated on the SO pin for which I wait to go low in my spi library. So that should be fine. I don't have the plot of the readout itself…
I ran into some issues using pdkProjectCreate script. See attached text files for output of both scripts i.e. pdkProjectCreate and pdksetupenv. The pdkProjectCreate script created a folder called MyExampleProjects but it was empty. The script appears…
Hello George,
Thanks for your replay.
Regarding the second warning test case:
Compiler version: TI v16.9.6.LTS [TI v18.1.1.LTS]
Build output:
**** Build of configuration Debug for project AutosarCanStack ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8…
Thanks George,
compiler version: TI v16.9.6.LTS [TI v18.1.1.LTS]
Here is the build console output:
**** Build of configuration Debug for project AutosarCanStack ****
"C:\\ti\\ccsv8\\utils\\bin\\gmake" -k -j 8 arch/arm-cortexM4/drivers/Can.obj -O …