Part Number: TM4C123AE6PM Other Parts Discussed in Thread: TM4C129XNCZAD , SEGGER Hi Team,
When we program the controller (TM4C123AE6PMIR) through CCS, board works properly.
But when I disconnect debugger and power cycle the board, program doesn't execute…
Part Number: TM4C123AE6PM Other Parts Discussed in Thread: EK-TM4C123GXL Tool/software: TI-RTOS Hi,
May i get any exmple codes for TIVA controller
Best,
Ugra
Part Number: TM4C123AE6PM i need to read/write to internal eeprom. Using EEPROMProgram() function causes some delay. that is why i need to use EEPROMProgramNonBlocking() function. Do i have to use interrupt when i use EEPROMProgramNonBlocking function? Is…
Part Number: TM4C123AE6PM
Hello everyone,
I need advice regarding some software design. Here is the quick explanation, I have some DAC which generates some analog signal as a response to some input square signal. It generates some small output wave which…
Part Number: TM4C123AE6PM Hi champs,
customer wants to have watchdog timeout of 1 sec.
He found, that wdog times out after 2 secs.
He is using tivaware, see below: *! frequency of separate timebase (16MHz) */ #define SRVSF_WDT_FREQ ((USIGN32)16000000u…
Part Number: TM4C123AE6PM Tool/software: Code Composer Studio Hi Folks,
I have a custom developed board with TM4C123A controller, that I debug via DK-TM4C129X. When I launch my program, the debugger stops at beginning of the main(), but I cannot place…
Part Number: TM4C123AE6PM Other Parts Discussed in Thread: BQ40Z50 Hello,
I currently have a customer with this issue:
"
We are shipping systems with the TI microcontroller TM4C123AE6PMI7R. In one of the uses, one of its I2C buses is connected to…
Part Number: TM4C123AE6PM Tool/software: TI C/C++ Compiler Hello everyone,
I have a question regarding CAN communication. I have two boards with TM4C123AE6PM and in both of them PA0 and PA1 are used for CAN and connected to CAN transceiver and I have set…
Part Number: TM4C123AE6PM Hi Folks,
I develop a brushed DC motion application, where I want to get the speed with direction from the QEI0. My problem is, that (for me, it seems) arbitrary number of times, discarding any periodicity, the direction flag…