According to our project, every code that is written needs to be tested, but we realized that most of the Tiva code is not testable (infinite loops, direct hardware access without layer structure...). Therefore, we thought we should rewrite the code in…
Part Number: TM4C123GH6PM Other Parts Discussed in Thread: EK-TM4C123GXL We are using your Keil uVision software as part of the Microprocessors course. The card we want to use is TM4C123GH6PM. The driver support link on your site ( www.ti.com/.../getliterature…
Part Number: TM4C123GH6PM Hi together,
we are currently checking if there is a built in measure in the TM4C 123 GH6 PMT for detecting soft errors in the memory such as bit faults (caused by environmental radiation).
Is there a built in detection measure…
Part Number: TM4C123GH6PM Going forward, please indicated, which IDE will support Tivaware and development using TM4C123GXL Launchpad?
Thanks and Best Regards,
Sudhir Gupta
Part Number: TM4C123GH6PM I want to generate sine wave using TM4C123GH with DAC MCP4921 , However i am not getting output at my IC port.. my code is as follow:-
#include <math.h> #include <stdint.h> #include <stdbool.h> #include "inc/hw_memmap…
Hi Charles,
Thanks for your replied.
Here I answer the question as below:
- In addition, what exactly is your ABA swap test?
Ans: I'm using a production test pass PCBA and swap with customer return board parts TM4C123GH6PM.
I can found that the failure…
Part Number: TM4C123GH6PM Hello,
I am using Keil uvision4 for programming. I have independently verified that SSI1 works fine as a SPI master. Next, I am trying to configure SSI1 of TM4C123G as a SPI slave device. My objective is to read in incoming SPI…
Part Number: TM4C123GH6PM Other Parts Discussed in Thread: UNIFLASH Hello ,I have problem with my TM4C123GH6PM and i hope that anyone can help me. i was uploading a simple code to the board using debugger option from CCS and by mistake the USB was unplugged…
Part Number: TM4C123GH6PM Other Parts Discussed in Thread: EK-TM4C123GXL I am currently using the TM4C123GH6PM microcontroller to develop a bootloader. During the bootloader development process, I need to modify the flash location in the 'tm4c123gh6pm…