Other Parts Discussed in Thread: TMS570LS3137 Dear team
Where can I find the design files for the TMDS570LS31USB ?
I checked at the following link with no luck.
https://processors.wiki.ti.com/index.php/Category:TMS570
https://processors.wiki.ti.com/index…
Part Number: TMDS570LS31USB Hi there,
I see that TMDS570LS31USB has a single CAN transceiver. And I have two TMDS570LS31USB.
So, I was thinking that I could hook up these two dev kits to have a CAN bus network.
What sort of cable do I need? a regular can…
Part Number: TMDS570LS31USB I have a driver issue with the XDS100 drivers. I have built a distributed test setup using 16 of the TMS570 MCU Development Kit (USB). I connect them all to a single Windows 7 PC via four USB hubs. My PC connects to the first…
An important note on the TMDS570LS31USB is: " All applications run on the Development Stick should be limited to 100 MHz HCLK Speed"
I am able to run my application at 160 MHz, but what is the reason/concern to restrict at 100 MHz?
Power? If so…
Hi TI
Where can I find the design files for the TMDS570LS31USB and TMDX570LS31CNCD development boards?
I need information regarding which MCU peripherals are accessible for external equipment.
best regards
Dennis
Refer to the schematic and peripherals that the HDK board offers . I am currently working with TMS570LS3137 HDK this has 8MB external SD RAM so all our code sits in external 8MB RAM and we are able to do large size files debug .
IF YOUR PROGRAM is…
Hi QJ,
Are you guys at TI Support able to run this Hercules_MCU_Bootloader.zip from processors.wiki.ti.com/.../TMS570_Hercules_MCU_Bootloader on a TMDS570LS31USB dev board?
The last thing I tried was to add "X" permission to SRAM since FLashAPI runs…
Part Number: TMS570LS3137 I am working on TMDS570LS31USB. I am utilizing F021 Flash API v02.01.01.
And I managed to erase flash sectors in bank 1 and program data in bank 1.
Odd thing is though erasing sector worked when I gave (160/2)Mhz as input frequency…
Hi Rocky,
The easiest way is using HALCoGen for generating two (or more) project for nodes. In the case of simplex communication (1TX -> nRX) you should enable at least one TX message on your transmitter node and one RX message on your receiver node(s…