Part Number: TMDSCNCD28M36 Tool/software: TI-RTOS Hi i am using TMDSCNCD28M36
and i got communicating with using LAN port which placed on the develop kit
Actually this would be kind of funny question
So what protocol now i am using?
ssh? snmpv2, snmpv3…
Part Number: TMDSCNCD28M36 Tool/software: Code Composer Studio there's some codes like downside ====================================================
void InitIpcDriver_C28()
{
// Step 3. Clear all interrupts and initialize PIE vector table:
// Disable…
Part Number: TMDSCNCD28M36 Tool/software: TI-RTOS Hi i'm using TMDSCNCD28M36 but i cant connect target by an error about XDS100v3.
the code is down.
Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the…
Part Number: TMDSCNCD28M36 Tool/software: Code Composer Studio
Error connecting to the target: (Error -151 @ 0x0) One of the FTDI driver functions used during the connect returned bad status or an error. The cause may be one or more of: no XDS100 is plugged…
Part Number: TMDSCNCD28M36 Tool/software: Code Composer Studio I'm testing program files downloading above Control Card(TMDSCNCD28M36) and I saw a codes including <xdc/std.h>, <xdc/cfg/global.h>......
And I found these files are placed…
Part Number: TMDSCNCD28M36 Tool/software: Code Composer Studio Hi this is a electronic troll again plz see my beautiful problem
before)
after loading M3
yes and the problem is i have nothing idea about whatsgoingon
and the last error code quote
Cortex_M3_0…
Part Number: TMDSCNCD28M36 Hello,
I am implementing a bootloader where it take Intel-base hex files in order to update both cores from the F28M36 CPU. The M3 part is fine, and I am facing an issue with the C28 FlashAPI.
Below there is the code that…