Part Number: TMDSDC3359 Tool/software: Linux Hi
I am trying to connect a TMDSDC3359 Data concentrator with two TMDSPLCKITV-4 CEN service nodes but the data concentrator does not recognize them.
is any problem of incompatibility?
How can i use the udpIPv6App…
Hi,
I am working with SOMPLC-F28PLC84 rev 1 (DC software version : 4.7.0.6, DC type : G3, DC DSP software version : 17.7.1.4).
The silent reboot configuration not working
./g3_mgmt_cli
Connecting to 127.0.0.1:20000
Connected… >>
>> cfg-dc –srf…
Part Number: TMDSDC3359 Tool/software: Linux Hi
I have a TMDSDC3359 data concentrator.
I want to configure it for a smart grid infrastructure. My guide document is the TI G3 DC Software User Guide, appendix C.
In the section 2 (prepare the sd card) there…
Part Number: TMDSDC3359 Hi,
My company needs a PLC Development kit which allows us to deploy communication between Data Concentrator and e-Meter. I want to know if the product TMDSDC3359 can help to achieve that goal.
The communication between the Data…
hi
i have an TMDSPLCKITV4-CEN and i want to configure the two modems as service nodes using a data concentrator TMDSDC3359. In the explicative video, the configuration is done with a V3 kit using RS-232 connection. The V4 dont have RS-232 interface. How…
Hi, i have an TMDSDC3359 data concentrator. When i introduce the ./PLC_setup.sh command to configure a PLC from the TMDSPLCKITV4-CEN as a node, the next error message is shown
-sh: ./PLC_setup.sh: No such file or directory
Where can i find that file? …
Part Number: TMDSDC3359 Hello TI, I work for the Isrel electric company in the field of Smart Grid PLC. We promote PLC communication projects based on PRIME and G3-PLC.
In order to establish a meter testing laboratory, using PRIME and G3 technologies…
Part Number: TMDSDC3359 Hello,
We've bought a TMDSDC3359 (revD) and we are trying to flash the G3 DC firmware using PLC_setup.sh tool but without sucess.
We have connected the PLC SOM to it's P2 connector and powered the board with the 12VDC source…
Part Number: TMDSDC3359 We're looking at using the AFE031 PLC chip. I'm trying to determine which PLC chip this eval board is using. http://www.ti.com/tool/tmdsdc3359#supportandcommunity