Part Number: TMDSDOCK28379D
Hello,
I had been using a TMDSDOCK28379D docking station for my project. While working, one of the GPIO pins (GPIO (one of 122, 124 or 126) accidentally came in contact with a +15 V supply pin from an auxiliary power supply…
Part Number: TMDSDOCK28379D Other Parts Discussed in Thread: TMS320F28335 , TMS320F28379D Hello, I am using a differential amplifier circuit to sense the voltage of a capacitor. The terminals of capacitor are directly connected to input terminals of differential…
Vincent Beaulieu-Gagnon said: I was able to make the led blink!
Great!
Vincent Beaulieu-Gagnon said: Now i have another question.
Should i build a new project and move stuff from the exemple i want to build on? (like here: https://www.ti.com/video/series…
Hello
Vincent Beaulieu-Gagnon said: Also, is it normal that i can't choose a board for the project?
The original syscfg file only had device information and not board information. Hence there is no option to switch the board.
Vincent Beaulieu-Gagnon…
Part Number: TMDSDOCK28379D We are having trouble using our TMS320C2000 development tool. When trying to test with CCS the example "led_ex1_blinky.c" using the following configuration
it gives us the following message:
I attach a photograph…
Part Number: TMDSDOCK28379D Other Parts Discussed in Thread: C2000WARE , TMDSCNCD28379D Where can I locate and download the BOM and Schematic for TMDSDOCK28379D DEMO Board?
Hi Pawan,
I created a new empty project from C:\ti\c2000\C2000Ware_5_00_00_00\driverlib\f2837xd\examples\cpu1\empty_projects\CCS.
Now i created a sysconfig and add it in the project folder.
Everything build fine:
For point 2, do i copie only these files…
Part Number: TMDSDOCK28379D Hi,
I am using the TMDSDOCK28379D for an application, and i dont need to use the pin from 121 to 180.
Also, i don't have the docking on my board for those pin (121 to 180)....
Is the card going to work well without de 5V…