Part Number: TMDSLCDK138 Other Parts Discussed in Thread: OMAP-L138 Hi,
Running the example MCASP_Audio_lcdkOMAPL138_c674xExampleProject an error while debug raised almost on the start of running, "Break at address "0xc3034d80" with no debug information…
Part Number: TMDSLCDK138 Hi,
During CCS11 session on EVM TMDSLCDKOMAPL138, trying to defined new ccs project template/example SYS/BIOS > TI Target > Minimal, the platform field was not defined, see images attached
Thanks,
Itzhak Kroin
Part Number: TMDSLCDK138 Other Parts Discussed in Thread: SYSBIOS , AM5728 , OMAPL138 , OMAP-L138 Dear E2E,
I have bought the OMAP-LCDK-L138 development board, installed CCS, installed C6SDK, installed MCSDK, read the Device User Guide, Read tons other documents…
Hello
Sorry for missing this post
Unfortunately we do not have any additional collateral that will help student development on this content.
As far as I understand these audio benchmark kits software was done for another device like K2G and will not work…
Part Number: TMDSLCDK138 Other Parts Discussed in Thread: OMAP-L138 , OMAPL138 Square Wave is getting severely distorted during a simple pass-through as shown in the screenshots attached (shown are distortions for 1, 10, and 1,000 Hz).
Bandwidth of interest…
Yes, I have used both the Line in and the loop back test is configured for the MCASP (2-16 bits) 32 bits data.
The first picture is a snapshot of the spectrum of both channels with not test running, but it shows only noise. No program is running.
During…
Part Number: OMAP-L138 Hello,
I am considering the OMAP-L138 Development kit (LCDK) for my design. I understand that t he LCDK does not have an onboard emulator. An external emulator would be required. From the hardware development section, I see that…
Part Number: TMDSLCDK138 I want to connect the TMDSLCDK138 evaluation board to a RGB LCD, is this possible with this evaluation baord?
I could not find any RGB outputs.
Part Number: TMDSLCDK138 Other Parts Discussed in Thread: OMAP-L138 , TMS320C6748 , OMAPL138 , Hello everyone,
I have some questions about these two development kits, processors on them and programming them by Code Composer Studio, maybe I overlooked some…
Part Number: OMAP-L138 Other Parts Discussed in Thread: TMDSLCDK138 I want to burn into my TMDSLCDK138 board default Linux image. Where can I download it?