Part Number: TMDSPREX28335 Hi TI team,
I used to use the digital control library (DCL) to realize a simple PI control algorithm. It worked when I used the 28335_RAM_Ink.cmd file to load the program in RAM. It also worked when I used the "F28335.cmd" while…
Part Number: TMDSPREX28335 Hi there,
I am studying the laboratory project provided in TMDSPREX28335 DSP toolkit. I want to delay a digital signal with a frequency of 3.75MHz to output after 2us, but the output flip rate of the IO port of DSP28335 seems…
Part Number: TMDSPREX28335 Other Parts Discussed in Thread: C2000WARE Hi, team
I am tring to get the phase difference of two signals whose frequency are up to 100kHz,I know using XOR gate circuit plus capture module of 28335 can do the job. But it seems…
Part Number: TMDSPREX28335 Other Parts Discussed in Thread: SN74LVC1G08 I have two external square wave signal with frequency of 100kHz, how can I measure the phasee difference with DSP28335?
Part Number: TMDSPREX28335 Other Parts Discussed in Thread: C2000WARE ,
I want to use the 2 DAC pin given on the explorer board for my Digital to Analog Converter. Please, anyone, provide me with the pin number of the DAC pins on the board.
Thankyou
Best…
Part Number: TMDSPREX28335 Hi Team,
Prompt error message
C28xx: Error connecting to the target: (Error -233 @ 0x0) The JTAG IR and DR scan-paths cannot circulate bits, they may be broken. An attempt to scan the JTAG scan-path has failed. The target's…
Part Number: TMDSPREX28335 Other Parts Discussed in Thread: C2000WARE Hi team, Since my customer can't post on the forum, I submit a question for him. "I am using a TMDSPREX28335 board and I am trying to dump two signals: 1) an external 50 Hz sinusoidal…
Hi Ankit,
No worries!
The 'ConfigCpuTimer()' function which both sets of code call actually sets the TIE bit to 1 in order to enable the generation of a timer interrupt (this is through the timer's configuration). If this bit is not enabled then…
Hello Mr. Pate,
Firstly, please accept my apologies for replying this late as I was busy with other activities related to my research and didn't get time to reply sooner.
I ran a few experiments of my own to get clarity on this, and, luckily I have…