Part Number: LAUNCHXL-F28069M Hello,
I am trying to connect a resolver to a Launchpad 28069M using a "TMDSRSLVR C2000 Resolver to Digital Conversion Kit". I follow ed the hardware connection proposed by Mathworks
de.mathworks.com/.../hardware…
Part Number: TMDSRSLVR Hi Team,
Is there any alternative to TMDSRSLVR which is obsolete?
Or, without using TMDSRSLVR, is it possible that convert the resolver signal to two phase output by the other products and then put it into the LAUNCHXL-F28069M?
…
Part Number: TMDSRSLVR Hi Team,
Can you please check and advise with following request:
"
When I look at the controlsuite now, I can find the schematic as TMDSRSLVR_v1.0. R2 is written on the kit we have. From this section, we understand that it is…
Part Number: TMDSRSLVR Hi, I would like to determine the rotor position by an analog sine / cosine sensor and became aware of the resolver library. Some specs: Application should run on a F28027 fixed controller. The expected maximum mechanical rotor speed…
Part Number: SM320F28335-EP Tool/software: Code Composer Studio I have implemented the resolver circuit based on TMDSRSLVR along with code, which successfully provides angle.
F28335 is running on 100MHz SYSCLK.
During debug, I note the LOS flags (Loss…
Part Number: TMDSRSLVR Dear team
I’d like to use the TMDSRSLVR kit for angular position sensing. Figure 2 of the following TI document indicates that it takes the R-Sin and the R-Cos signals as inputs, and the R-Excitation (R-Ex) as an output. www…
Part Number: TMDSRSLVR Hello,
I am developing some code for a resolver interface and I am porting the code for the resolver for a f28335 (controlSUITE\development_kits\TMDSRSLVR_v1.0\Resolver_f28335) to a TMS320F28379D.
I believe I understood most of…
Part Number: TMDSRSLVR Hi,
The excitation voltage is generated by filtering the PWM signals from the MCU and it's a clean unipolar sine wave. There are two questions:
1. Can you provide documentation for the circuit design for components parameter…
Hello,
For resolver:
There is a resolver as part of TIDM-02014 ( https://www.ti.com/tool/TIDM-02014 ) - I suggest taking a look at the schematics of this design for an example analog front-end.
TMDSRSLVR SW can serve as a code example (C:\ti\controlSUITE…