Part Number: TMDSSGI-EVML138 Other Parts Discussed in Thread: OMAPL138 , AM1808 Hi Team,
Our customer is looking for the design files such as schematic diagram and PCB layout of TMDSSGI-EVML138 development kit. I found the E2E thread below which provides…
Part Number: TMDSSGI-EVML138 Other Parts Discussed in Thread: OMAP-L138 Tool/software: Linux i'd like to use gre tunnel
but it seems that a gre package is not included in opkg.
i tried to configure gre tunnel :
->ip tunnel add gretun1 mode gre remote…
Other Parts Discussed in Thread: CC1101 , CC1120 , CC1190 , CC430F5137 I am interested in using Smart Grid Infrastructure Evaluation Module (TMDSSGI-EVML138).
I have the following questions:
1. The Evaluation Module is compatible with Evaluation Boards…
I need to know the following information when working with the SGI EVM Board as a data concentrator and the PLC KIT 3000 (TMDSPLCKIT-V3) as slaves.
1. Distance range.
2. Modulation type.
3. Electric power.
4. Operation frecuency band.
5. When…
I am interested in using Smart Grid Infrastructure Evaluation Module (TMDSSGI-EVML138).
I wonder if GPIO can be used int the TMDSSGI-EVML138.
If possible, please let me know how to use GPIO in the TMDSSGI-EVML138.
Thanks in advance.
Hello,
We are using DVSDK to environment to build the application for EVML138 target. When we try to build an application which uses “llibxerces-c3.1” i amgetting linker error because this library does not exist in dvsdk. So question is
How to install…
Part Number: AM1808 Other Parts Discussed in Thread: OMAPL138 Hello,
We are planning for AM1808 MPU for development. But we have seen a special note like below in Product description.
Special note
For new designs, consider the AM3352 Sitara Processor…
I am using the Smart Grid EVM Revision E (TMDSSGI-EVML138). It is the one located here: https://store.ti.com/TMDSSGI-EVML138-Smart-Grid-Infrastructure-Evaluation-Module-SGI-EVM-P2739.aspx
I see the daughter board in the image but I do not have it…
I am using SGI EVM Board (http://www.ti.com/tool/ tmdssgi-evml138 ) with the Linux distribution that comes with it. It is call Arago Project.
I would like to run the prime_dc program on startup. I already created the script that runs the program, but…