Part Number: TMDSSOLARPEXPKIT Hi!
I have 4 questions.
1)is Piccolo-based Solar Explorer Development Kit suitable to the PV panel with given specs in images? 2) I am wandering whether TMDSSOLARPEXPKIT has built-in solar PV panel emulator by use of DC power…
Part Number: TMDSSOLARPEXPKIT Tool/software: Code Composer Studio I am using TMDSSOLARPEXPKIT and I want to know RMS Voltage value, but the VrmsReal, which is calculated by SineAnalyzer Module is really unstable. For example, when I have at the output…
Part Number: TMDSSOLARPEXPKIT Hi!
I have 4 questions.
1)is Piccolo-based Solar Explorer Development Kit suitable to the PV panel with given specs in images? 2) I am wandering whether TMDSSOLARPEXPKIT has built-in solar PV panel emulator by use of DC power…
1. przes_fdbvac must be 9
2. Make sure Vac_FB has 1.65 offset to be able to connect to the ADC
The module should synchornize and has been used sucesfully on multiple project.
Also confirm that in IQmath file you have selected fixed point MATH Type
Part Number: TMDSSOLARPEXPKIT Hello,
The TMDSSOLARPEXPKIT has a supplied battery charging example - but for the TMDSSOLARCEXPKIT (Concerto F28M35Hx Control Card) - there isn't one.
Just wondering why the kit either doesn't have that and/or I can't find…
Part Number: TMDSSOLARPEXPKIT Hello, Just confirming -- can the controlSUITE "High-voltage Solar Maximum Power Point Tracking Development Kit" software be used for this EVM? And, in general, can this be used with all other Piccolo EVMs? Thank you…
Part Number: TMDSSOLARPEXPKIT Tool/software: Code Composer Studio Hello I am working with TMDSSOLARPEXPKIT, but I want to use version v1.2 instead of v1.0. I add files to includes folder and initialize macro, but I receive errror like this:
"../F28035_FLASH_SolarExplorer…
Part Number: TMDSSOLARPEXPKIT Is it possible to change PWM type in this kit? Or it is only possible to control it by unipolar modulation?
What about bipolar or hybrid, which are included in SolarExplorer_HWguide.pdf?
Part Number: TMDSSOLARPEXPKIT Is it possible to generate higher frequency PWM on this kit?
Do I need to use HREPWM then?
I want to adopt this kit to really low output Power and still synchronizing with the grid. So the current will be less than 10mA.…
Part Number: TMDSSOLARPEXPKIT When I try to run build 2 my Gui_PanelPower does not follow the The Gui_PanelPower_Theoretical after setting Gui_InvStart to 1. I also have Gui_Vpv equal around 0,8.when the SW1 is on. Any ideas?