Other Parts Discussed in Thread: TMS470MF06607 Hello TI, I am using iSystem's external debugger iC5000 ( www.isystem.com/.../tms570-tms470m-rm4) with TMS470MF06607 HDK When I plug-in the debugger to ARM-JTAG connector DS1 LED turns ON which is a clear…
Other Parts Discussed in Thread: UNIFLASH Recently we bought a TMDX470MF066HDK from digikey. After we installed the software that came with it we tried to run "Hercules Safety MCU Demo" Application and get the message No demo board found . When…
Hello,
I am new to the TMS470 and have just obtained an HDK.
I was going to use the button (S1 on the board) but discovered that there is no mention of S1 anywhere in the manual! I also discovered that there is also no schematic either. Searching around…
Other Parts Discussed in Thread: TMS470MF06607 , HALCOGEN
Sirs,
Does the TMS470MF06607 start execution if the external clock is missing? I assume the XTAL on the OSCIN pin is broken *before power-on*.
Or the part switches the clock source to the HFLPO and…
Other Parts Discussed in Thread: TMS470R1B1M , TMS470MF06607 , SM320F2812-HT I am designing a control system for high temperature (175C). A microcontroller that qualifies for this is SM470R1B1M-HT. Before I design and manufacture the system I’d like to write…
Hi,
I have set FMzPLL = 80 MHz = VCLK
The VCLK2R = 0 so peripheral clock should be VCLK/2 = 40 Mhz. But when I measure the SPI data bit SPI2, the bit waveform as below, the bit rate is only 1 Mhz. Why the transfrom is 80:1?
Hi
I am using TMDX470MF066HDK eval board and try to use SPI for I2C control. I just write a 2 word length in buff and send it out. But I always watched 128 bit length data and clock from SPI2 pins. My source code as below:
unsigned short SPI_data…
The ARM JTAG (20 pin) connector on the TMDX470MF066HDK is not for programming other devices. It is for using an external emulator to program the on-board device. Pulling the JTAG_SELn pin low disables the on-board XDS110. To program the device on your…