Hi,
i dont know how to configure the CAN for different baudrate.
i want how to calculate the bit timing calculations for CAN.
http://www.ti.com/tool/tmdx470mf066hdk
thanks
arun
Vikas,
>>Can i not program other TMS470MF06607 microcontroller using this development board?
According to the TMDX470MF066HDK page, this kit has a XDS100v2 Onboard JTAG debugger that allows you to flash and debug the device using CCS.
>>Can I…
Part Number: TMS470MF06607 Other Parts Discussed in Thread: HALCOGEN Hello TI,
Development board : TMDX470MF066HDK Hercules Development Kit
I am using HET to generate a PWM signal. The driver level code of HET is generated from HALCoGen. My application demands…
Hi Chuck,
Thank you for the reply. But when i checked with Mathworks website there it is mentioned that support for TI TMS470 is available. Is there any other board other than TMDX470MF066HDK Hercules Development Kit .
Other Parts Discussed in Thread: MSP430F2272 , MSP430F1612 , DRV8823 Dear All,
I am working on a research funded project on Adaptive Lightning system in Automobiles, ( TI Reference Design “ SPRUHP3 – July 2013” ). We are using two boards TMDX470MF066HDK…
I measured the voltage on a pines:
MyDevice | TMDX470MF066HDK
RST (pin98): 0.3V 1.5V
TEST (pin97): 0V 0V
VCCP (pin95): 3.3V 3.3V
ENZ (pin91): 0V 0V
PORRST (pin98): 0.3V …
Dear Chuck-san,
Thank you for your quick reply.
As to your question, please see the below.
* TI EVM customer using : TMDX470MF066HDK
* Measurement point of VCCIOR and VCC : Customer measured the both VCCIOR and VCC at the device pin.
* JTAG interface…
Other Parts Discussed in Thread: HALCOGEN Hi,
I am running FreeRTOS on TMS470M development kit (TMDX470MF066HDK). Currently, my code compiles without errors, but when I load it on the processor and run it, it frequently ends up in a hard fault exception…
HI
In TMS470MF066HDK, there is already CAN transreceivers in the development board but for LIN it is not there.
whether a separate LIN transreceiver will be required for TMS470MF066HDK ?
Thanks
Vikas