Part Number: TMDX654GPEVM Hi Team,
Our customer bought TMDX654GPEVM but he noticed that the silicon revision of AM6548 is 1.0. Please see the picture of the board below for reference. He would like to ask for a replacement board with AM6548 revision 2.0 or …
Andrew,
Sorry for the delayed response. I did not see the pcie were brought up in the linux log you sent earlier. Could you confirm which silicon revision you will be using for your final product? If using SR2.x, I suggest you use the SR2.0 IDK and latest…
Part Number: TMDX654GPEVM Hi Experts,
Good day.
We would like to ask your assistance to confirm the following queries for TMDX654GPEVM:
1. What OS can the product run on? 2. Are you expected to ship with a pre-installed OS? 3. Is the software download and…
Part Number: TMDX654GPEVM Hi Experts,
On the Scripting Console of CCS 10.4.0, executing the launch.js of pdk_am65xx_07_03_00_54 and pdk_am65xx_08_00_00_36 gives the following error:
js:> load("C:\\ti\\pdk_am65xx_08_00_00_36\\packages\\ti\\drv\\sciclient…
Part Number: TMDX654GPEVM Hi,
We are doing boundary scan on TMDX654GPEVM board using XJTAG tool. 1. It has 3 ethernet PHYs, out of which 2 are connected on PRG2 RGMII interface (U88 and U31) and 1 is connected on MCU RGMII interface (U22). We are able…
Exactly. To be more specific:
Michael Krummsdorf said: Select PER1_PLL as signal source for OBSCLK: mw 0x00108000 0x5
was wrong in this case as this changes OBSCLK clock source while divider is clkdiv+1 = 1.
Replace the above command with:
Divide OBSCLK…
Part Number: TMDX654GPEVM When I received the EVM board, the TI SDK included on the SD card was 05_01_00_11. The bootloader/kernel included in that pre-built package is the only version I have been able to get to work. I've tried the 07_01_00_17 pre-built…
Part Number: TMDX654IDKEVM Other Parts Discussed in Thread: TMDX654HSEVM , TMDSLCD1EVM Hello Guys,
Our customer is planning to order one of these boards but is confused as to which of the three should they choose from. They cannot accurately identify the…
Part Number: TMDX654GPEVM Tool/software: Code Composer Studio Request : How to change the speed of command 5A by DDR mode of octal flash at TMDX654GPEVM
Octal flash specification : The speed of 5A command ( to read SFDP) at DDR mode should be 86Mhz with…
Hi Renan,
My apologies
Here are the answers and some additional questions
1)How to check my demo system operate? Do they need to buy a master TSN or not?
TI : That will depend on what you need in TSN. Which profile ? Which set of protocols.
2) What is…