Hi, I'm currently using TMDXEVM8168 for my embedded linux project. Is this EVM board support Jumbo Frame? If Yes, how should I do to enable it & test it?
The GigE PHY used in this board is L-ET1011C2-C-D from LSI.
The layout data of the TMDXEVM8168 Rev. E evaluation board is available for download, unfortunately it is in binary Cadence Allegro format. I would like to import this into Altium Designer, but this requires an Allegro installation.
Is there anybody…
I have bought TMDXEVM8168 with DDR3 memory, 702390-1001 REV D 08 SEP 11, but unfortunately it missed SD card which contains documents, drivers and software. I got no printed document. I have asked the local company through which I bought to arrange the…
Other Parts Discussed in Thread: AM3894 Hi,
Understand that most but not all Gig Ethernet support Jumbo Frame. Thereofre would like to double confirm that TMDXEVM8168 is Jumbo Frame supportable. The project development is AM3894 based. Thanks.
Regards…
Hi
all,
Can anyone provide me with the FPGA co-processing
interface options provided by tmdxevm8168 EVM - DM816x/C6A816x/AM389x Evaluation
Module . Primarily I would like to make the EVM tmdxevm8168 off load some of its video signal processing t…
I owned a TMDXEVM8168 and now I'm following a document "TI816x-PSP-04.00.00.10-FlashingTools". This is to burning NOR Flash using CCS in Window XP. At page 4, I was asked to create a target configuration file called "ti816x_usb.ccxml". However, there…
Other Parts Discussed in Thread: TVP7002 I have a DM8168 application where video capture over DVI or YCbCr is required. According to this link below:
http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/p/139681/503946.aspx#503946
…
Other Parts Discussed in Thread: OMAPL138 , TVP5158
Hi all,
Iam trying to identify processor + evaluation platform for 3d vision processing application. Have to decide on a development setup which is flexible enough to allow
- dual camera support (synchronous…
Hello,
A heat sink and its fan is observable on the top of TMDXEVM8168. Are these parts necessary for the whole range of DM816x/C6A816x/AM389x processors? If not, which ones could be used in a fanless system board?
Regards, Gaston
Other Parts Discussed in Thread: TVP5158
Hi all,
I am trying to identify dual camera setup for tmdxevm8168 EVM - DM816x/C6A816x/AM389x Evaluation
Module . EVM TVP5158EVM for
multi camera interface says it can perform " Digital Video/Audio Outputs…