Part Number: TMDXIDK437X Hi,
I would like to confirm my calculation of the adc range.
what is the range of the adc in the idk am437x? is it 0-3.3 ? other ?
what is the value in volts I expect to see when nothing is connected ? is it 1.65 ? other ?
what…
Part Number: TMDXIDK437X Hello.
I apologize for repeated questions, I have already raised a similar topic here.
https://e2e.ti.com/support/processors/f/791/t/881329
Unfortunately for me the question has not been completely closed. I read the documents…
Part Number: TMDXIDK437X Hi,
I have an issue with editing the pinmux file :
I edit the pinmux file idkevm_config.pinmux and replace the files ( am43xx_idkevm_pinmux_data.c and am43xx_pinmux.h
with the new files.
than I tried to build the PDK.
when doing so…
Part Number: TMDXIDK437X
Hi,
I am trying to add quadrature encoder support to the IDK motor control example.
after fiddling around I have narrowed my question to the following :
right after the board init , if I add the following lines , the SW crashes…
Part Number: TMDXIDK437X
Hi,
I am looking for a code example AM437x ADC - simultaneous sampling of both ADC for the purpose of motor control, and could not find any.
I am trying to sample both ADCs and have "Start convert" signal depend on a timer to…
Part Number: TMDXIDK437X
where can I find the pinmux file that is associated with the motor control project example ?
is this is the file (assuming default installation folder)
C:\ti\pdk_am437x_1_0_16\packages\ti\starterware\tools\pinmux_config\am43xx…
Part Number: TMDXIDK437X
Hi ,
when I use TwinCat , it can find the ethercat device , but when I scan for boxes , I get an error
"unknown device type found"
vendor id 0 , product id 0 , revision number 0
what am I doing wrong?
Part Number: TMDXIDK437X
Hi,
Software:processor_sdk_rtos_am437x_5_02_00_10 PRU-ICSS-EtherCAT_Slave_01.00.07.02 PRU-ICSS-Industrial_Drives_01.00.02.03
The sampling of the adc signal needs to be done using the pru core to load the pru_adc_sampling_bin…
Dimitry,
I was discussing with the HSR/PRP developer: Rx/Tx test is only meant to be run with specific frames which are prepared and sent by the application. This was meant purely for off the box demonstration of redundancy feature. It might misbehave…