Part Number: TMDXIDK437X Tool/software: TI-RTOS Hello
I want to configure IDKAM437x to work with PRU and cpsw ports. For PRU, I use the driver icss_emac, for PRU I use cpsw_nimu_eth. For initialization, I use the following code:
PRUICSS_pinMuxConfig…
Part Number: TMDXIDK437X Tool/software: TI-RTOS Hello In my project, I am trying to change the function location section using void myFunc (void) __attribute__ ((section (". AppCode"))) ; I want to change the memory area from DDR to OCMCRAM. I compile…
Part Number: TMDXIDK437X
Hello,
I have two questions related to TIDEP0025.
1, From the document, it seems to be nesessary to download EtherCAT slave stack and access the source file.
If we are not ETG member, Are there any information how to run…
Part Number: TMDXIDK437X Hello,
Can I ask you to specify exact versions of download files to try "motor_control_AM437x_arm" project?
I tried to find my best answer. There are four items, but some questions were remaining:
(1) EtherCAT Slave…
Part Number: TMDXIDK437X
Hi,
I use the Peripheral Interface of the PRU on AM437 to receive asynchronous data that is send from another PRU on the same controller. I send data at a clock of 100kHz and the receiver runs at 800kHz so that I have 8x oversampling…
Part Number: TMDXIDK437X
I use the motor routines inside sysbois run motor (and the level is level2 :#define LEVEL2 2 // Verify ADC, park/clarke, calibrate the offset),The motor only turned a bit to stop, and then "motor error" lights on the light…
Hello TI,
One of my customer is going to use a Sitara device in their design. They will purchase the TMDXIDK437X development board:
We know this has a Linux variant that will run on it.
We are looking for insight as to whether the Linux OS that comes…
Hello,
I've got AM437x IDK board ( TMDXIDK437X ) and I want to use onboard CAN interface.
I want to build some example application but I don't know how.
Example included in SYSBIOSSDK-IND-AM437X v02.00.00.02 is not working on this board.
I also…