Part Number: TMP100-Q1 Other Parts Discussed in Thread: TMP100 Hello,
On our board, we have a TMP100 sensor with one pull-up resistor on ADD0, and ADD1 is floating.
Therefore, we expected a slave address of 1001111 (0x4F). During our test procedure…
Part Number: TMP100-Q1 Other Parts Discussed in Thread: TMP100 Hi Expert,
I am looking for the IBIS model of TMP100AQDBVRQ1, but could nt find any.
Please help me out on this .
Regards,
Abhinand
Part Number: TMP100-Q1 Hello,
In our application we cannot leave any pins floating. They must all have a discharge path and in the case where a "float" level is needed, we have to provide an external resistor divider to ensure the level stays within bounds…
Part Number: TMP100-Q1 Other Parts Discussed in Thread: TMP100 , , TMP101-Q1
Hello, using TMP100 in a simple temp reading without using ALERT signal, we noticed in datasheet, TI recommend issuing a general call command via i2c as follow
7.3.8 General…
Part Number: TMP75B-Q1 Other Parts Discussed in Thread: TMP100-Q1 , TMP75-Q1 Hi team,
It is described in TMP100-Q1 datasheet as below that General call reset is required if supply voltage
is not sure to be <0.3V.
#1. Does it also apply for TMP75-Q1 device…
Part Number: TMP100-Q1 Hi team,
I was wondering if you could help with the following question about a specification in the TMP100-Q1 data sheet (SBOS581A –SEPTEMBER 2011–REVISED MAY 2017).
In section 7.5 Electrical Characteristics under Temperature…
Part Number: TMP100-Q1 Can the TMP100-Q1 SCL and SDA pins be pulled up to a voltage lower than the V+ chip supply pin? Section 9.2.1 of the datasheet mentions "The SCL, SDA, and ALERT lines can be pulled up to a supply that is equal to or higher than…
Part Number: TMP101-Q1 Other Parts Discussed in Thread: TMP100-Q1 , spec only specifies POL bit default value after power up, I need to know other bits too:
SD ?
TM ?
(don't have the part on hand just to read it)
Part Number: LM73-Q1 Other Parts Discussed in Thread: TMP100-Q1 , SYSCONFIG , TMP100 I need a reference design to interface LM73C0QDDCRQ1 with microcontroller. Please assist for the same.
Part Number: PROCESSOR-SDK-AM62X Other Parts Discussed in Thread: AM625 , AM623 , SYSCONFIG Hello,
We have design 2 king of bord base on AM62x SK EVM board.
One design is using AM623 with 2x2GB of DDR4, the other design use AM625 with 2x1GB.
I configure…