Other Parts Discussed in Thread: WL1835MOD , WL1271 Hi
So I'm trying to get Wifi+BT functionality on a custom board using WiLink8 (WL1835MOD). The CPU is a TI AM335x. We use a custom distribution built with Yocto.
After enabling debug messages I finally…
bootlog040419.txt hi,
please find the attached log for analysis.
yes, streaming video is halted.
Similar case not occured in EVM, hence we cannot share the log.
BR
satya
We are still having trouble with WL8 bring up on the system described in this post . We are using the default boot binaries from AM57x Processor SDK 3.0 and we're getting the below error about wlcore_sdio not being loaded when we run configure-device…
here is the kernel .config I am using at present #
# Automatically generated file; DO NOT EDIT.
# Linux/arm 4.4.19 Kernel Configuration
#
CONFIG_ARM=y
CONFIG_ARM_HAS_SG_CHAIN=y
CONFIG_MIGHT_HAVE_PCI=y
CONFIG_SYS_SUPPORTS_APM_EMULATION=y
CONFIG_HAVE_PROC_CPU…
Hi Eyal
yes you are right our custom board has taken influences from both the beagle bone black and the EVM.
I thought I had attached a boot log file to my original post. I will attach another here as I have recompiled the kernel with dynamic debug…