Part Number: TMP104 Other Parts Discussed in Thread: TMP144 , TMP144EVM We have a test setup with a MCU and TMP104YFFT. But we could not get the correct temperature reading from TMP104. We do not know what is the problem. Attached is the test result log…
Part Number: TMP104 Hello guys,
One of our customers is going to evaluate TMP104YFFR on their own board. They need answers to the following questions for soldering.
Q1. Are the surface and core material of the solder ball (solder bump) on the device package…
0363.main.c
/* --COPYRIGHT--,BSD
* Copyright (c) 2013, Texas Instruments Incorporated
* All rights reserved.
*
* Redistribution and use in source and binary forms, with or without
* modification, are permitted provided that the following…
Other Parts Discussed in Thread: TMP104 Hi,
My customer will use multi TMP104 chips to setup a temperature sensing network in servo motor system. If we have any EMC test report or suggestion for TMP104, you could share with me.
Temperature compensation…
Other Parts Discussed in Thread: TMP104 I'm using the tmp104 device on an evaluation kit that is our manufacture. It is connected to the USART of a STM32L4 processor (ARM Cortex-m4) configured for autobaud @ 57600,8,N,1 and I have a console application…
Other Parts Discussed in Thread: TMP104 Hi,
I have two quick questions from the customer and the information on the datasheet seems ambiguous.
Within the communication protocol between host and tmp104s, does the calibration command have to be sent every…
Other Parts Discussed in Thread: TMP104 Hi,
I am looking for TMP104 Temp error graph versus operation temp.
I found this on the datasheet but It only shows -40 to 125 degree
I need extended chart in operating temp. range which is -55/150 degree
Thank…