Part Number: TMP116 Hi Sir,
If my customer wants to do the TMP116 self-calibration on their PCBA, just follow the methods in section 8.1.1.2. Is that right?
Part Number: TMP116 Hello,
My customer would like to know if TMP116AIDRVT can pass the ultrasonic cleaning process after manual mounting on PCB.
Please advise, thanks.
Part Number: TMP116 Hello,
Let our customer knows the difference between TMP116 and TMP116N.
Pricing wise I can expect TMP116N is lower grade accuracy.
However what is exact meaning of the datasheet statement between "TMP116 accuracy without calibration…
Part Number: TMP116 Dears,
We are using digital temperature sensor chip TMP116AIDRV, one IIC bus is mounted with two temperature sensors, STM32F405 is used to drive. IIC is simulated by IO port, IIC pull-up resistance is 4.7K, 100K clock is used, and…
Part Number: TMP116 Hi Expert,
My customer are using C2000 to communicate with TMP116 by I2C, ADD0 pin is connected to SDA, seem from the I2C waveform, C2000 send correct device ID waveform which is 1001010x, and command 0x0F, but TMP116 send back 0xffff value…
Part Number: TMP116 Does TMP116 support reading/writing multiple registers in a single I2C transfer? Many I2C devices allow the base register to be selected and additional registers accessed by clocking additional bytes.
For example: If I start read…
Part Number: TMP116 Hi,
With TMP116 temperature sensor driver we are able to read the raw value of temperature, Please provide if any formula available to extract actual temperature from obtained raw value.
Thanks,
Nikhil K