Part Number: TMP116 Hi,
1m harness is used to connect the TMP116 and the control board.
(1) Please teach if there are any precautions or countermeasures when routing I2C/SPI with a harness.
(2) Currently, we are considering placing a bidirectional logic…
Part Number: TMP116 Hi team,
Could you give me comment on following customer question? The customer plans to use waterproof coating on the PCBA after mounting TMP116.
Q1. If TMP116 has any restriction on waterproof coating material for PCBA or caution…
Part Number: TMP116 We are using TMP116 on an I2C bus mastered by i.MX6Quad, and used with a Linux operating system. On rare occasion after reboot or power cycle, the Linux system gets a TMP116 driver error after trying to read the CFGR register. Most…
Part Number: TMP116 The TMP116 datasheet states that a unique ID is stored in the EEPROM to support NIST traceability.
Does this imply that we can also receive the individual validation/calibration measurements of each individual device based on the…
Part Number: TMP116
Hello, Say that I have a TMP116 that is continiously powered off and on. To perform the oneshot mode, I have to write 11 to MOD (Which was 01 as it had to be in shutdown mode). Should I call a general reset (Or just power it off and…
Part Number: TMP116 Hi team,
My customer is evaluating TMP116 and plans to implement it in FPC. Epoxy adhesive is used to fix the temp sense FPC on detection object.
There are 2 types of use cases.
a) Epoxy adhesive will cover all the package in 60C temp…
Part Number: TMP116 Hi E2E,
Having an issue with the read back on a TMP116 device ID, expecting 116 from the 0h0F register, getting 126 back.
Not seeing this on all sensors either, a subset of newer sensor are exhibiting this issue. Any suggestions…